Resorts World Las Vegas
In a city where revenue is measured by the square foot, Resorts World is the largest hotel property built on the Las Vegas strip since 2011. From the 117,000 sq. ft. casino to more than 3,500 rooms, and all points in between, an integrated technology experience and a first-rate connectivity solution was essential to the hotel’s success.
The goal was to help Resorts World Las Vegas build a state-of-the-art property with a focus on guest and employee experience. Corning was able bring a fiber-rich, fully integrated network with 5+ connected devices to each room. For a large technology-heavy hotel venue such as this hotel, a traditional network would require hundreds of telecom rooms. By using Corning® Network Solutions, the hotel only needed 24 telecom rooms.
Download the full case study PDF and be sure to see what’s possible for your network by checking out Corning’s technology solutions for the Hospitality Industry.