SD-LAN | Software-Defined Local Area Network | Corning

Fully Managed, Future-Flexible Enterprise SD Network

For ultimate flexibility and visibility to the edge of your network, Corning’s Fully-Managed Software-Defined LAN (SD-LAN) Network Solution is built on the future-ready foundation and long-reach capabilities of our ActiFi® Composite Cable and Intelligent Power Solutions. As technology plans grow and evolve, network demands become more complex. We designed our SD Network specifically for enterprise and to meet the demands for an optical fiber network solution.

Our fully-managed SD-LAN solution can be integrated by our approved Everon® Partners. 

SD-LAN - Fiber to the Edge Network Architecture: Architectural diagram of a Corning SD-LAN showing a centralized software-defined network controller managing fiber and power delivery to the network edge

Advantages of the SD-LAN Solution

Advantages of the SD-LAN Solution

Adapt as Network Requirements Change

Corning’s SD-LAN solution is flexible by supporting two transport technologies within the same platform. Our dual-mode solution supports both point-to-multipoint (PON / GPON / XGSPON) and point-to-point (Active Ethernet), allowing for maximum adaptability as technology needs change.

Scale & Expand Your Tech Strategy
With a future-ready infrastructure in place, your enterprise can seamlessly scale to add more devices as your technology strategy evolves without having to pull additional cable.

Extend Your Network Reach to Save Space and Cost
Deliver connectivity beyond 2,000 feet or more. Reclaim revenue-generating space by reducing telecommunication rooms. Reclaim technology funds by reducing TR build-out and maintenance costs.

Simplify Network Management
Maximize your time with a single pane of glass orchestration platform that allows for template-based provisioning, remote troubleshooting, and visibility to the very edge of the network. Contact your local Corning Sales Engineer for a demo of our Advanced Orchestration and Management Platform.

What is Software-Defined Networking?

Software-defined networking decouples hardware and software. Specifically, it separates control logic which is centralized from forwarding logic which remains on the hardware. The hardware is often referred to as a whitebox because its functionality is programmable.

End-to-End Solution

Innovation is in our DNA. From the day we introduced the first viable low-loss optical fiber in 1970, we have been building on this innovation by expanding our in-building network expertise. In addition to our broad portfolio of cable, connectivity, hardware, and intelligent power, Corning also specializes in network actives and software, including:

 
SDLAN Whitebox appliances (1G/10G/40G Optical Switching Fabrics and PoE, PoE+, and PoE++) with a full SFP portfolio
 
SDLAN Intelligent software-defined access nodes for optical to Ethernet conversion and PoE
 
SDLANs Advanced SD Network Orchestration Software

 

SDLAN
Network Savings for medium office, large office, campus, senior living, hotel with Corning SD-LAN

LAN Educational Resources

Abstract background with connected lines and dots

Fiber to the Edge Knowledge Center

Fiber to the Edge Knowledge Center

The FTTE knowledge center is your one-stop source for information on Corning's array of solutions and products for software-defined solution, remote powering and more.

The FTTE knowledge center is your one-stop source for information on Corning's array of solutions and products for software-defined solution, remote powering and more.

LTE 4G 5G New generation fast speed mobile internet connection

Fiber to the Edge Network Architecture Enables a Wireless World for Infinite Innovation

Fiber to the Edge Network Architecture Enables a Wireless World for Infinite Innovation

If an enterprise has increased bandwidth and lower‑latency requirements on its radar, it has an opportunity to put an end to costly, disruptive, and inefficient Category cable network upgrades—and instead make a smarter network investment.

If an enterprise has increased bandwidth and lower‑latency requirements on its radar, it has an opportunity to put an end to costly, disruptive, and inefficient Category cable network upgrades—and instead make a smarter network investment.

fiber at Corning

Go Farther with Fiber

Go Farther with Fiber

Corning SD‑LAN, combined with fiber’s superior reach and virtually unlimited bandwidth, enables networks to be more adaptable, scalable, and programmable.

Corning SD‑LAN, combined with fiber’s superior reach and virtually unlimited bandwidth, enables networks to be more adaptable, scalable, and programmable.

Contact me today to discuss SD-LAN deployments!

We are here to help you with any questions about your in-building network. Fill out the form below and one of our representatives will be in touch. 

Thank you for your inquiry!

One of our representatives will be in touch with you shortly.