Senior living communities are adopting more technology to provide a comfortable, connected, and engaged experience for their residents, guests, and employees. Corning’s in-building fiber to the edge solutions can simplify network management and enable the technologies that are transforming senior living communities.
Connectivity for Senior Living Communities: A Case Study
Extend the Reach of your Network to Enable Remote Devices
Whether a senior living facility is a campus-style with multiple buildings or offers all services under one roof, enabling remote applications like security cameras, door locks, and outdoor Wi-Fi can be a challenge. Corning’s remote power solutions and ActiFi® composite cable deliver data and power beyond 2,000 feet to enable remote devices that are often hard to reach or far from the nearest intermediate distribution frame (IDF) closet. As a result, senior living communities can reduce the number of IDF closets needed and repurpose that saved space to become revenue generating spaces, such as providing room for additional beds.
Add Network Flexibility for Unique Application Requirements
Technology plays such a big role in the resident experience, and having a flexible network that can support the unique requirements of a wide variety of devices and applications is key. The Corning solution provides added network flexibility by supporting both passive optical network (PON) and point-to-point active Ethernet transport technologies under the same streamlined infrastructure.
As a result, senior living communities do not need to pull additional cabling to support the different application needs at the edge. Corning’s software-defined local area network (SD-LAN) adheres to the standard IEEE networking protocols while adapting to meet various application requirements.
Simplify Network Management
Reduce troubleshooting time and easily manage IP applications at the edge with Corning’s software and orchestration platform. This platform provides visibility of the end-to-end service path directly to the edge, reduces provisioning time with template-based provisioning, and provides real-time and historical analytics. As a result, network managers benefit from simplified day-two support and are able to resolve issues quickly to improve resident service.
Reduce Elopement Risk
Maintaining resident independence while also improving wander management is important as costly elopement-related insurance claims are happening more often1. The Corning software and orchestration platform supports transport layer security (TLS), allowing residents to maintain access to their own private network while moving throughout the facility. The system also helps staff members to quickly locate residents who need assistance.
Limit Resident Disruptions with a Future-Ready Network
Rather than rip-and-replace cabling to keep up with evolving technologies, leveraging a fiber and power-deep network can reduce day-two upgrade costs, prevent congested cable pathways, and limit resident disruptions during upgrades.
Getting Started
Corning can help you build a next-generation LAN that can support the specific needs of your senior living community. Contact your local Corning sales engineer or visit corning.com/fiberdeep for more information.
Solution Benefits
Everon® Network Solutions
Fiber to the Edge – Horizontal LAN
Learn More: Fiber to the Edge – Horizontal LANThe edge of your network is facing unprecedented bandwidth and mobility demands. We have solutions – including some you may not have considered.
Traditional LAN - Fiber in the Riser
Learn More: Traditional LAN - Fiber in the RiserThe fiber optic backbone is your network’s foundation. It connects various buildings and devices together to create the local area network. We have solutions for both outside plant and in-building applications that are available, compatible and easy to install.