Secure Fiber Optic Network Infrastructure Solutions for Military and Defense | Corning

Supporting the Future of Defense Technology

Supporting the Future of Defense Technology

At Corning Optical Communications, we take pride in our commitment to providing cutting-edge solutions for secure and robust communication networks. Our Fiber to the Edge (FTTE) products play a pivotal role in supporting the Department of Defense (DoD) and its mission to enhance network capabilities.

Corning is dedicated to advancing defense technology by promoting the integration of cutting-edge technologies. This commitment extends to ensuring high-bandwidth, low-latency connections for critical operations, security, and resilience across various applications. Reliable network capability is vital for the success of initiatives, safeguarding sensitive data, and adapting to the dynamic landscape of technology in defense.

The Defense Industrial Base is using fiber to drive modernization. DoD must do the same.

Our NextGen Data Transport Architecture, built with fiber, enables the Base of the Future to support virtually unlimited data loads and mission requirements with no need for refreshes. Here’s why our solution stands out:

  • Existing copper infrastructure cannot support increasingly data-dense military applications and weapons systems.
  • Current DoD networks are being swamped, with bandwidth constraints growing exponentially.
  • Copper is a limiting factor beyond 10 Gbps and will inhibit future mission growth.

Corning’s data transport architecture is specifically designed for higher bandwidth requirements, security, flexibility, and lower cost – exactly what DoD requires.

Corning is proud to announce that our state-of-the-art Assured Services Local Area Network (SD-LAN) portfolio of products has been approved on the Department of Defense Approved Products List

Our SD-LAN solutions represent the cutting edge of network technology, providing the DoD with secure, scalable, and adaptable network infrastructure. With Corning's SD-LAN, the DoD can rely on advanced solutions that enhance mission-critical operations, bolster security, and ensure seamless adaptability in an ever-changing landscape of defense technology. Explore our DoD-approved SD-LAN products to discover the future of network capabilities and security.

Search the Approved Products List >

DODin APL Logo

New Solutions + Proven Technology Deliver Benefits Across the Board

Mission Owners – Bandwidth Ready Now for Current and Future Weapon Systems

• High data throughput allows multitudes of additional ports ready for new missions

• More secure data transport because there is no EM signature

• Enhanced network monitoring possible through network orchestration

• Data scale does not matter, providing support for current needs and in the future without typical expense and disruption of upgrades

Installation Engineers – “Future-Proofing” Facilities

• Significant cost savings to install, operate, and upgrade

• Remote power embedded in cable means no separate A/C power required

• Future capabilities installed now enable the future with a fraction of the servers, cabling, closets — fewer runs, less labor, less configuration time

• Sustainable solutions translate into less power/cooling needed

• Wireless flexibility provided in labs, depots, shipyards, backshops, flightline maintenance, mission support facilities, etc.

Comms/IT – Building a 21st Century Network With Cyber Threat Resilience

• Future network flexibility with SD-LAN, minimizing network disruption

• Technology neutral approach supports active P2P Ethernet and PON

• Zero trust extends the access layer policy to the edge port, 802.1X, authenticate everything

• Single-pane-of-glass orchestration allows integrated management of multi-tenant services

• Network visibility provisioning delivers automation from edge ports to WAN

• Network Source of Truth provided through central controller/policy, continuous audit, automatic remediation and alert anomalies

Unparalleled Reliability
Our technologies offer unmatched reliability, reducing network failures and downtime.
Security Beyond Comparison
Corning's solutions enhance the DoD's security posture by providing secure, difficult-to-tap communication infrastructure.
Scalability and Adaptability
Corning's AS-LAN products are designed to scale as needed, supporting the DoD's evolving network requirements, including support for zero trust architecture.
FTTE Solutions for Edge Computing
Corning's FTTE products bring fiber optics closer to the end-users, enhancing network performance and responsiveness.
Deployment in Challenging Environments
Corning's solutions are field-tested and suited for remote and challenging locations.

Corning Optical Communications is committed to helping the DoD remain at the forefront of defense technology

Discover why Corning is the trusted choice for government agencies. With over 30 years of experience, we deliver the secure and high-performance network infrastructure that mission-critical operations demand. Our future-ready fiber network solutions ensure the reliability and speed of deployment needed for sensitive military communications and security systems.

In the full DoD solutions document, you'll find valuable insights into our commitment to providing comprehensive technical support, from design assistance to fiber optic training, helping you stay ahead of change in a world where failure is not an option.

Explore how Corning empowers you to safeguard the nation's well-being with dependable, secure, and cutting-edge network solutions.

Download Now >

Additional Resources

Not quite sure what to do next? Our specialized Federal sales team is here to help.

Contact us today by filling out the form.

Thank you for your submission!

We will be in contact with you soon.