Fiber to the Edge (FTTE) is a local area network (LAN) architecture that utilizes optical fiber to deliver data to the edge of the network. At the edge, the network interfaces through ports or wirelessly via cellular or Wi-Fi with Internet of Things (IoT) devices—such as cell phones, laptops, security cameras, machine-to-machine controls, building management systems, automated guided vehicles, and more—as well as the applications that support them.
What is Fiber to the Edge (FTTE)?
What is Fiber to the Edge (FTTE)?
Who should use a Fiber to the Edge architecture?
Who should use a Fiber to the Edge architecture?
FTTE is ideal for businesses that need high capacity and flexibility in their network. Optical fiber delivers the high bandwidth, low latency, reach, and flexibility required to meet the demands of developing applications, like next-gen Wi-Fi, high-availability A/V, and 5G within a single building or across a large campus.
How does Fiber to the Edge work?
Like every enterprise IT network, an FTTE-based LAN consists of active optical components (e.g., routers, switches) and passive optical components (e.g., cables, connectors).
In a traditional enterprise LAN IT architecture, data is transmitted either entirely via copper or through a combination of a fiber backbone and copper to the edge, requiring equipment closets, or IDFs, throughout the network. An FTTE architecture is fully optical, with optical fiber carrying all data transmissions. This design allows the network to operate from a central equipment room, or MDF, eliminating the need for IDFs. The extremely high bandwidth provided by an FTTE architecture enables wireless operation of many edge devices, reducing the need for individual wiring and porting.
Power for an FTTE-based LAN can be supplied through separate copper electrical wiring or composite cabling that contains both fiber and copper. This approach delivers both data and power to the edge, or POE, directly to devices such as wireless antennas, cameras, and point-of-sale systems at distances greater than 100 meters (328 feet).
An FTTE-based LAN can be managed using traditional, decentralized hardware options or through software. A software-defined LAN consolidates all system data, making it accessible via a computer or mobile phone screen—a feature often referred to as a “single pane of glass” interface. This allows the network to be monitored, controlled, and updated virtually.
Benefits of Fiber to the Edge (FTTE) for Enterprise IT Networks
Benefits of Fiber to the Edge (FTTE) for Enterprise IT Networks
- Extremely high bandwidth and low latency
- Increased security
- Reduced complexity
- Lower installation and lifetime cost
- Space efficiency
- Reduced environmental impact
- Power over distances beyond 100 meters (328 feet)
- Scalability for a variety of building and campus sizes
- Flexibility for the future
Corning® Everon® Network Solutions for your Enterprise
Let's talk about Everon® Network Solutions
Whether you need help with current data demands or planning for the future, we can help.
Complete this form to get started today.
Thank you!
Thank you for your inquiry. One of our representatives will be in touch with you shortly.