Modern data centers adopt Spine-Leaf architectures to handle East-West traffic and invest in infrastructure for growing bandwidth demands. For cost-effective and rapid deployment, they utilize fully factory-terminated cabling options in Main, Horizontal, and Equipment Distribution Areas.
Revolutionizing Data Center MPO Connectivity
Revolutionizing Data Center MPO Connectivity
However, traditional MTP® connectors face challenges in buried conduit installations for connector protection and organization. The form factor of the MTP® connector, well optimized with push-pull boot for traditional structured cabling, is not ideal for highly-dense packaging and easily to install in conduit solutions with near-max fill ratios.
Corning and US Conec Ltd. introduced the Fast Track™ MTP® Connector as part of the EDGE™ Rapid Connect solution to address these challenges and drive data center connectivity innovation further. This factory-terminated data center interconnect solution offers high-density packaging and connector protection, eliminating the need for splicing while maintaining optical performance.
Utilizing Fast Track™ MTP®, EDGE™ Rapid Connect accommodates up to 3 x 3456 fiber cables in a 10 cm conduit, with a waterproof pulling grip. Time studies show significant efficiency, allowing two technicians to fully mate both ends of 3456 fibers in one 8-hour workday.
The Evolution of the MPO/MTP® Connector
The Evolution of the MPO/MTP® Connector
Read more about the Evolution of the MPO/MTP Connector by clicking on the dates below.
-
1988 - NTT released the MT Ferrule
Since NTT released the MT Ferrule as a pre-engineered splice into commercial subscriber lines in 1988, MT Ferrule technology has evolved to answer multiple challenges in the market. In the 2000s, with the emergence of the MPO (Multifiber push-on) connector, data center installers and designers were able to increase fiber density and decrease installation time by switching from single fiber or duplex connectors to multi-fiber connecters in an 8 or12 fiber form factor. In addition to fiber density, as the transceiver roadmap increased from 10G to 40G requirements, parallel optics, introduced multiple fiber lanes for data transmission. This multi-lane method of sending and receiving data heralded a greater need for an efficient means of interconnection.
-
1996 - US Conec Ltd. released the MTP® connector brand
In 1996, US Conec Ltd. released the MTP® connector brand — a family of advanced MPO connectors designed for 4, 8, and 12-fiber ribbon applications. That same year, the MPO format was standardized by the International Electrotechnical Commission (IEC) and embraced by an industry thirsty for a better way to install, deploy, and manage high-density fiber networks. Corning adopted the MTP in its Plug & Play™ cable portfolio for backbone, cross-connect, and breakout applications.
-
1999 - Low-insertion-loss MTP® Elite connector introduced
In 1999, US Conec Ltd. introduced low-insertion-loss MTP® Elite connector components that not only improved on insertion loss from 0.75dB down to 0.35dB for single-mode applications and 0.60dB down to 0.35dB for multi-mode applications, but also reduced the sensitivity of the connector bodies from accidental bumps or pulls on the cable jacketing through a floating ferrule technology that allows the connector end-faces to remain in contact while the bodies can rotate relative to each other. It uses tight-tolerance elliptical guide pins to improve guidance and reduce performance-impacting ferrule pin bore wear and degradation. Corning was able to build on this technology to introduce the EDGE™ product line, an industry-leading, low-loss, high-density cabling solution that delivers premier optical performance and reliable signal power.
-
2021 - Fast Track™ MTP enables EDGE™ Rapid Connect
In 2021, US Conec Ltd. designed a state-of-the-art connector having two rows of 12 fibers (2x12f) that brought simplified use to the MPO format by offering a small-profile, field-installed connector, all while leveraging the proven features and technology of US Conec’s MTP® connectors. With a novel design focused on simplicity and reliability, the small-profile of the Fast-Track MTP connector enables a reduced-size pulling grip for installation through restricted pathways. Corning, once again, leveraged this technology to deliver a new solution to the market in the form of EDGE™ Rapid Connect: a factory terminated, high fiber count cable solution that eliminates splicing and reduces installation time by 70%.
“Fast-Track MTP Connectors pack an extreme-density punch, and they plug in for the same low-loss connection every time.”
Steve Jenkins, Data Center Foreman, Litewave Communications
Real life examples of the Fast Track MTP and EDGE Rapid Connect?
Real life examples of the Fast Track MTP and EDGE Rapid Connect?
Our case study is loaded with real world metrics and examples, resulting in a savings of up to 70% on installation time when installing trunk cables between data center buildings.
Tools & Resources
Bill-of-Materials Tool
Bill-of-Materials Tool
Forget the guesswork. We can help you select the fiber optic and copper products you need for your enterprise network or data center with our configurable online bill-of-materials tool.
Forget the guesswork. We can help you select the fiber optic and copper products you need for your enterprise network or data center with our configurable online bill-of-materials tool.
Learn MoreSee the Light® Training Program
See the Light® Training Program
We are committed to educating our customers, providing quality real-world fiber optic training on latest products and applications, ensuring you will always receive the most up-to-date and industry specific knowledge.
We are committed to educating our customers, providing quality real-world fiber optic training on latest products and applications, ensuring you will always receive the most up-to-date and industry specific knowledge.
Learn MoreAuthorized Distributors
Authorized Distributors
Corning works in close cooperation with a wide range of qualified intermediaries including installers, distributors and network design planners throughout EMEA. Our distributors have robust programs for end users, contractors and installers and are ready to support your needs.
Corning works in close cooperation with a wide range of qualified intermediaries including installers, distributors and network design planners throughout EMEA. Our distributors have robust programs for end users, contractors and installers and are ready to support your needs.
Read MoreCore Products Guide
Core Products Guide
As a leader in data center technology and innovation, we understand the unique requirements of the data center and have compiled this guide to provide you with that valuable information at your fingertips. The guide includes product details and a list of resources that can save you both time and money.
As a leader in data center technology and innovation, we understand the unique requirements of the data center and have compiled this guide to provide you with that valuable information at your fingertips. The guide includes product details and a list of resources that can save you both time and money.
DownloadNetwork of Preferred Installers
Network of Preferred Installers
Our innovative network-style program connects your business today to the tools, solutions, and rewards that you need for a more profitable tomorrow.
Our innovative network-style program connects your business today to the tools, solutions, and rewards that you need for a more profitable tomorrow.
Learn MoreLet’s connect. Our experts are here to support every step of your way.
Whether you need help with your current implementation or planning for the future, we can help. Complete this form to get started.
Thank you for your submission!
A Corning representative will be contacting you shortly about your inquiry. Should you need immediate assistance please call our customer service line at +49 30 5303 2100.