Hyperscale, Cloud Data Center, AI & Big Data | Corning

Empowering Big Data, AI & ML with Advanced High-Speed Network Solutions

Empowering Big Data, AI & ML with Advanced High-Speed Network Solutions

Hyperscale and cloud data centers form the backbone of today's digital world, fueling the growth of AI computing, machine learning, and big data and shaping the future of network design.

Since 2024, we have seen a remarkable surge in optical links and connections to processors, reflecting the growing interest in generative AI, and other AI-enabling technologies. This growing demand necessitates hyperscale operators to deploy smaller, denser fibres and small form factor connectors with increased efficiency. The quest for resiliency, scalability, and agility in network design is a central part of this digital transformation.

As pioneers in the field of fibre optics, we are proud to be part of this journey towards the future, by offering a broad array of cable and large-scale, highly adaptable or customized connectivity solutions geared to provide on-demand IT capacity whenever and wherever it is needed.

As AI continues to reshape industries, reliable data transmission is essential to its success. Corning, a pioneer in optical fiber technology, offers GlassWorks AI™ — a range of solutions and services designed to support the evolving needs of AI-driven networks. Learn more and connect with an expert from Corning’s GlassWorks AI team.

Let's Connect!

Network Connectivity for Hyperscale Data Center Halls

Network Connectivity for Hyperscale Data Center Halls

Embrace the AI revolution with Corning's EDGE™ and EDGE8® solutions, and innovations to meet extreme density, reducing labor and waste, and enabling transitions to 800G, 1.6T and beyond.

EDGE™ Distribution System (EDS)

EDGE™ Distribution System (EDS)

Revolutionize your server row cabling with Corning EDGE™ Distribution System, designed for up to 75% faster installations with a single pre-engineered assembly.

View Solution

Corning Configured Rack

Configured Racks

Simplify data center deployment with Corning's sustainable pre-assembled racks, featuring reduced packaging and an eco-friendly design.

View Solution

Pre-loaded Housings

Preloaded EDGE™ and EDGE8® Housings

Experience seamless integration and rapid deployment that simplifies your processes with a significant reduction of 55% in packaging weight for a greener, more sustainable future.

 

EDGE™ Preloaded Housing >

EDGE8® Preloaded Housing >

VSFF Duplex Optical Connectors for Next-Gen Networks

VSFF Duplex Optical Connectors for Next-Gen Networks

New very small form factor connectors, like the MDC (Mini-Duplex Connector) are paving the way for higher density duplex connectivity and supporting speeds of 400G, 800G and beyond.

View Solution

MMC Connector Solutions

MMC Connector Solutions

MMC connectors (16F and 24F), compact powerhouses, offer three times the higher cabling port density than MTP® formats to help data centers quickly expand to accommodate high-bandwidth AI applications.

Learn More

Data Center Interconnect Options for Hyperscale Data Centers

Data Center Interconnect Options for Hyperscale Data Centers

Our preterminated EDGE™ Rapid Connect or semi-preconnectorized DCI solutions provide seamless data transfer for hyperscale data centers, meeting bandwidth needs and simplifying installation.

Explore our high-density Corning® Cables with Flow Ribbon Technology, reducing the cable diameter diameter by up to 60% and accommodating up to 6.912 fibers.

We’re here to support hyperscale and cloud data center needs

We’re here to support hyperscale and cloud data center needs

Corning assists in offering the service, quality, and value expected in a high-performing, high-density solution. We provide a wide variety of products from the outside plant cable to the data center interconnect and hall environments, enabling:

Rapid deployment
for low- to high-density
applications
Adaptive infrastructure
solutions to migrate to higher-speed technologies and integrate new interfaces in existing footprints
Full-service
from network design to engineering to post-installation support
Large-scale manufacturing
capabilities to quickly deliver products helping you meet your installation timeline

Hyperscale Data Center Frequently Asked Questions

Have additional questions about hyperscale? Contact us today!

  • What is difference between hyperscale data centers and traditional data centers?

    The simplest way to compare hyperscale data centers vs. traditional data centers is by their size and scalability. Hyperscale data centers are designed with density and performance at a scale that can be up to 1000x greater than an enterprise-style data center. Hyperscale data centers benefit from economies of scale, despite their incredible appetite for power, cooling, and fiber, and therefore are able to offer services a traditional data center cannot. Traditional data centers rely more on manual processes, and are typically built with custom designs tailored to specific organizational needs.

  • What effect has the rise of generative AI had on fiber optic data center networks?

    To meet the computational demands of Generative AI, big data analytics and other AI-like applications, customers now require a new fiber-rich second or “backend” network to connect GPUs. As a result, networks require over 10 times more optical fiber compared to legacy server racks.

  • What is a backend network and why do data centers need to consider them in their planning?

    In the context of Generative AI, the backend network often refers to the server-side infrastructure that powers the algorithms to generate new content. This could include deep learning models, such as Generative Adversarial Networks (GANs), which learn to create new data with the same statistics as the training set, e.g., images, music, speech, or text.

    The backend network related to Generative AI involves several elements, including Data storage and management, processing power, model training, and deployment.

  • What is a neural network?

    A neural network is a group of interconnected units that send signals to one another. In the field of AI machine learning, a model or program will use interconnected units called “neurons” or “nodes”, to process data in a way similar to the human brain.

Tools & Resources

Let’s Connect. Our experts are here to support every step of your way.

Whether you need help with you current implementation or planning for the future, we can help. Complete this form to get started.

Thank you for your submission!

A Corning representative will be contacting you shortly about your inquiry. Should you need immediate assistance please call our customer service line at +49 30 5303 2100.