Seasoned industry professionals may recall the excruciating, painstaking days of installing and connecting countless fibers, one at a time. As the number of data centers grew exponentially in the 2000s, designers and installers were tasked with managing hundreds and even thousands of single- and 2-fiber connector solutions. To accommodate the high volume of connectors within ever-tighter space constraints, installers and designers were forced to create more elaborate storage and routing solutions that came with their own set of challenges.
Fortunately, those days are long gone – thanks in large part to the emergence of the multifiber push-on (MPO) connector. The MPO format dramatically reduced the amount of time, effort, and space required to install and deploy network technologies, particularly in parallel optic applications.
Even beyond its value in the parallel optics space, a closer look at the MPO format reveals the full scope of its applications. To get a better understanding of big picture and true value of MPOs, we must start at the most logical place: the beginning.