Many stem cell companies use small-scale cultures, such as 6-well plates or flasks, to quickly develop initial processes for stem cell production and meet early milestones. When it comes time to produce stem cells on a larger scale, new factors come into play. Choosing the right extracellular matrix (ECM) coating and process is critical to scale-up success.
Here's a closer look at bioreactor scale-up, other options for scaling up stem cell production, and some coating considerations for large-scale production.
The Challenge of Scaling Up Stem Cell Production
Stem cell companies and laboratories may eventually need to produce much larger volumes of cells than those used in research and development. For example, a cell-based therapy company may need to go from 200,000 cells to inject into a mouse to 200 million cells to inject into a human patient.
The cells in the final product need to be high-quality and consistent, and they need to retain the safety and therapeutic characteristics that were demonstrated at smaller scales. It's important not to underestimate the complexity of this feat. In particular, increasing scale brings in considerations such as cost, cell health, and cell fate, and the choice of coating influences each of these.
As explained by Robert Padilla, a field application scientist at Corning, the way scale-up is implemented can have a huge impact on stem cells' destiny. "It's not just about cell attachment and health," he said. "There are also many signaling aspects that affect what the cells will become. The cardiomyocytes you're trying to grow could be pushed into a neural lineage. So, you need to make sure scale-up doesn't change the product."
Scale-up vs. Scale-out
Options for massively increasing the volume of adherent stem cells include stacked vessels, bioreactors, and microcarriers.
Stacked vessels, like Corning® CellSTACK® and HYPERStack® vessels, consist of stacked flasks or plates that are connected for easier filling and maintenance. Corning Field Application Scientist Whitney Wilson explained that stacked vessels are more accurately called "scale-out" solutions because they replicate the same conditions cells experienced in small-scale culture but multiplied many times. This makes the transition to large-scale culture more straightforward.