Rural areas come with a unique set of challenges. For one, low population density and long distances between homes make it less economically feasible for providers to build out to those areas.
On top of that, geographic and environmental barriers — including rugged terrain and frequent flooding — make network resiliency and repairability are critical factors in design decisions. In the past year alone, we’ve seen more than 30 trees fall and damage cables, so simple, speedy repairs are just as important to factor in as the initial deployment.
Using plug-and-play connectorized solutions, we were able to eliminate up to 80% of the splicing labor, significantly speeding up network installation and reducing the cost of splicing from $40,000 to nearly zero. And it’s not just at the deployment phase where these solutions make things easier, we’ve been able to get coverage back up and running after major storms within 24 hours thanks to the ease of repairability that comes with this technology.
Scaling for the future through collaboration
To date, we've connected more than 400 homes — and there’s a huge opportunity for expansion. By the end of 2026, we aim to pass 6,000 homes, supported by the New York State ConnectALL grant and the Municipal Infrastructure Program (MIP). In these cases, projects depend on tight deadlines to qualify for funding, which makes faster deployments an even higher priority. The “speed-to-market" capability that comes with Corning’s plug-and-play solutions allows homes and businesses to connect to the system within those tight time constraints.
The faster broadband deployments, combined with our community engagement efforts, also play an important role as we look ahead. When residents are informed about how the service works and what to expect, we tend to see pre-enrollment increase. And our ability to quickly roll out service led to a higher take rate. If our potential customers have to wait 3-4 months for service, we lose that momentum. But with Corning’s products, our customers can have service the very next week.
At Southern Tier Network, connectivity is at the heart of what we do, and Corning’s innovative solutions have completely transformed how we deploy broadband. Their pre-terminated FlexNAP cables and easy to use Evolv terminals have streamlined our process, allowing us to drastically reduce splicing labor, speed up installation timelines, and cut costs. These technologies have enabled us to meet tight deadlines, scale projects efficiently, and deliver reliable, high-speed internet faster than ever before. With Corning’s solutions, we’re not just building networks — we’re building a foundation for future growth and success in our community.