FRECAP’s standout feature is its eight independent cable entry segments. Think of it like eight triangular slices of pizza or pie. Those segments are individually gel sealed, which means cables are more resilient to disruptions during re-entry into the closure. With snap-and-seal gel technology in each segment, tools like screwdrivers, heat guns, or sticky tape are no longer needed, simplifying installation and maintenance in the field. Additionally, an integrated gel-sealing ring improves reliability for the entire closure as well as speed of installation.
It’s not just installation that’s streamlined — re-entry is up to 50% faster with FRECAP than with other closures, minimizing the risk of costly service interruptions and enabling more efficient network expansion. FRECAP’s design reduced the risk of disruption, ensuring long-term dependability and consistent performance.
Designed with technicians in mind, FRECAP is also compatible with widely used splice trays, allowing crews to work with a familiar interface while benefiting from faster, more streamlined installation.
Preparing networks for what’s next
While reliability is the top industry priority, the ability to future-proof and continue expansion is also top-of-mind. As connectivity demands accelerate, increased splice capacity and adaptability are essential. FRECAP can hold 33% more splice trays that other closures, increasing the overall splicing capacity and enabling network operators to expand without additional closures or vaults.
Its increased capacity and versatility allow it to function as a single closure that’s adaptable across multiple applications — from fiber-to-the-home builds to long-haul data center interconnects. This flexibility reduces deployment complexity and streamlines inventory and SKU management.
Keeping critical networks up and running
In a world where demands for network reliability are of the utmost importance, the Evolv FRECAP Closure helps operators maintain the integrity of their existing fiber networks while staying ahead of growing demand. In critical environments where downtime is not an option, FRECAP is designed to deliver the resilience required to keep operations running smoothly.
Click here to learn more about Corning’s innovative fiber closures and solutions or fill out the form below to speak with one of our experts.