Bringing Fiber to the Northern Frontier | Rural Fiber Deployment to Remote Northern Regions | Corning

How Corning Helps Deploy Broadband in Remote Regions

Barry Walton 
Published: June 26, 2025

As a Canadian native, I’m used to the colder weather. But environmental challenges in remote areas like northern Canada and rural Alaska are about more than just the temperature when it comes to deploying fiber broadband. Limited road access, unpredictable wildlife, and community buy-in add to the challenging landscape of far North American regions.

Communities stretched across the tundra or in the mountains face a digital divide that’s exacerbated by the landscape itself. In Canada specifically, only 78.2% of rural communities have access to high-speed internet, compared to 95.4% of the country overall. For remote rural communities, fiber broadband is more than just lightning-fast internet — it’s a vital lifeline  to education, health care, job opportunities, and cultural preservation.

But rural fiber deployments, especially in regions with harsh environmental challenges, face an added layer of difficulty. With any deployment, having a plan is key to getting the job done efficiently and effectively — but it's even more important in regions with so many external factors to consider. Manufacturing the fiber is just one part of what we do at Corning: successful deployments come from careful planning and close collaboration every step of the way.

What makes fiber deployment in Northern regions unique?

With unique terrain comes distinct challenges. Between the tundra, permafrost, and mountains, deployments need to be engineered around the instability of frozen ground and shifting terrain. Fiber builds in Alaska and Canada’s Northern regions operate completely differently than urban or even suburban deployments. The communities are small and often hundreds, if not thousands, of miles apart. And with limited road access, many of these rural Northern areas can only be reached by barge in the summer or float plane year-round.

From the moment we start planning, we’re thinking about how much cable is needed to reach just one location — and more cable is needed to stretch across these vast landscapes. Because of the sprawl and small communities, there also tends to be a shortage of trained labor in remote areas, which poses logistical challenges of flying in and housing teams, along with transporting materials.

On top of the vast geography, extreme cold weather and limited daylight create seasonal working constraints, making the building season much shorter than in warmer climates. Weather impacts both safety and deployment strategies.

Coordinating with local communities is about respect, not just logistics

And it’s not just geographic and climate challenges that have to be considered. These regions are also home to indigenous communities and sensitive lands. In Canada, it’s important to collaborate with First Nations communities, many of whom view broadband as next-generation infrastructure. Co-ownership models are growing in popularity, and they require trust, communication, and permitting for a successful deployment in those communities. On our end, we aim to offer solutions that are fast to install, easy to use and require minimal tooling and training to help create streamlined partnerships.

In Northern regions, wildlife can pose a different kind of “traffic management” challenge than in other areas. There's a deep respect for animals like elk, bears, and wolves, and it is important to work with local wildlife managers and First Nations contractors who assist in site safety to keep humans and wildlife out of harm’s way. Having that local knowledge is critical to successful deployments.

Designing for resilience and efficiency

In most Northern regions, there's only a brief window of workable weather — sometimes just a few months long. Every hour counts, so crews aim to minimize labor-intensive splicing.

Corning’s FlexNAP™ system is a game changer for projects like these. Rather than building connections in the field with traditional splicing methods, FlexNAP comes pre-connectorized, so customers can save time and simply plug-and-play. There’s no need for a full splicing crew, and this method requires fewer tools and less training than legacy solutions, which is crucial with a short season and a lot of ground to cover. Because the FlexNAP system comes on a plastic cable reel, it’s also easier to transport, as plastic cable reels are lighter than wood and can be moved without heavy machinery.

Extreme cold, snow, and high winds are facts of life in the north, and networks must be designed to withstand the elements — and be easy to fix if something goes wrong. That means fewer potential points of failure and systems that can be repaired without specialized tools. Corning’s design minimizes these risks and simplifies repairs, so if something breaks, you can unplug and replace it, rather than needing to bring in a full crew for repairs.

Deploying fiber broadband in rural Alaska and other northern regions requires a strong game plan and deep collaboration with local communities to help overcome vast distances, extreme weather and rough terrain. Pre-connectorized solutions are key to mitigating some of the area’s toughest constraints and building networks that aren’t just efficient to deploy but resilient and easy to maintain. In these regions, fiber deployments aren’t just about connecting cables — they’re about respecting a unique landscape and closing the digital divide.

Barry Walton

Barry Walton is in his 48th year in telecom and serves as Senior Broadband Solutions Advisor for Corning Optical Communications. In his current role, Barry is focused on developing and implementing innovative solutions to reduce labor in deploying fiber to the home in rural communities. His expertise lies in business case creation, operations planning, large-scale network planning, cost reduction, and deployment strategies for successful access network builds. Barry is one half of the #BroadbandGuys duo on LinkedIn, posting engaging content about Corning’s solutions to the challenges of rural fiber deployments.

Interested in learning more?

Contact us today to learn how our end-to-end fiber optic solutions can meet your needs.

Thank you!

A member of our team will reach out to you shortly.