Next Generation Optical Components and Solutions

Deploying Robust and Scalable Co-Packaged Optics Fiber Infrastructure

Deploying Robust and Scalable Co-Packaged Optics Fiber Infrastructure

Co-packaged optics (CPO), by merging optics and electronics, brings about a revolution in data center design, significantly enhancing power efficiency and bandwidth density. As the demand for higher bandwidth data processing capabilities increases with the rise of applications such as AI and machine learning, CPO technology offers a scalable solution that can adapt to these evolving needs. Learn more about co-packaged optics here.

Corning and Broadcom have collaborated to develop this white paper, which delves into insights and expertise, with a specific focus on the emerging field of co-packaged optics. The revolutionary CPO technology is reshaping high-bandwidth switches and distributed-computing hardware in data centers. The paper explores the design and handling practices developed over decades to ensure high reliability when using optical fibers, with a specific focus on emerging CPO designs. It also discusses challenges that manufacturers may face in adapting to this new infrastructure, particularly in terms of reliability and deployment. Download the whitepaper, Deploying Robust and Scalable Co-Packaged Optics Fiber Infrastructure, today to gain a deeper knowledge to navigate the complexities of CPO technology and harness its potential in your data center architecture.

Download the White Paper >

Discover Integrated Optical Solutions for 400G and Beyond

Discover Integrated Optical Solutions for 400G and Beyond

The growing demand for data and the challenges faced by data centers, such as reducing power consumption and cost per bit, have increased the significance of Corning’s co-packaged optics (CPO). CPO technology, which involves integrating optical components into switch boxes, holds great potential in addressing these challenges. While progress has been made in developing electronic components for CPO, the successful implementation of CPO technology also depends on the design and development of optical system solutions. Specifically, optimizing the complete optical system requires tailored optical components and effective management of the fiber within the switch box. Corning is a key component to the innovation and adaptation of CPO and Fiber-to-the-Chip (FTTC) on-board connectivity technology. 

Managing waveguides plays a crucial role in co-packaged optics. The fiber array unit (FAU), responsible for aligning fibers to waveguides, becomes more critical in CPO applications. Achieving low coupling losses requires tight positional tolerances and well-centered cores. Higher-fiber-count FAUs, such as those with 32 or 64 fibers, are needed to accommodate the higher densities in CPO. Manufacturing FAUs for CPO should consider polarization maintaining fiber (PMF) orientation and polarization extinction ratio (PER) maintenance, while retaining the high intrinsic reliability of the fiber. Experience in manufacturing FAUs for telecom settings can be advantageous due to similarities between CPO and telecom applications.

Scalable Fiber Solutions for Co-Packaged Optics (CPO)

In this webinar, industry experts from Corning and Broadcom explore key design considerations, fiber handling practices, and effective deployment strategies for navigating the emerging field of Co-Packaged Optics.

Watch Now