MTP Connectors | MPO Connector Advantages | Corning

Take advantage of the time savings, space efficiencies, and simplicity synonymous with the MTP® brand of MPO connectors.

Take advantage of the time savings, space efficiencies, and simplicity synonymous with the MTP® brand of MPO connectors.

In the early days of the industry, connecting fibers was a tedious and time-consuming task. With the rise of data centers in the 2000s, managing hundreds or thousands of single- and double-fiber connectors became a challenge. Elaborate storage and routing solutions were created to accommodate the high volume of connectors in tight spaces.

However, the introduction of the multifiber push-on (MPO) connector drastically reduced installation time, effort, and space requirements. MPO connectors have a wide range of applications beyond parallel optics. To fully appreciate the value of MPOs, it is important to start from the beginning.

Multiple Fibers Mean More Challenges

At the heart of the MPO connector lies mechanical transfer (MT) ferrule technology, originated by a leading Japanese telecom company in the mid-1980s for use in its consumer telephone service. This MT ferrule technology became the basis for the first MPO connector, introduced in the early 1990s.

The timing couldn’t have been better. Networks were being tasked with transmitting more data, more quickly. As the need for bandwidth increased, the industry began moving toward networks and cabling with higher fiber densities – the multilane highway of data transmission. This heralded the beginning of what is known today as parallel optics, or optical transmission using multiple fibers. Because of the increase in “lanes” used with parallel optics – the number of fibers moving data back and forth – an efficient, high-density interconnect was needed. The MPO connector format succeeded in establishing a compact means to efficiently couple and decouple the high-density MT ferrule format via a bulkhead-mounted coupler. More fibers, however, also meant more installation considerations.

MTP Connector Cross-Section including MTP Connector, Pins, and MTP Adapter

MTP Connector Cross-Section

MTP MPO Connectors: Less Time. Less Space.

Before the MTP connector came to market, it typically took two installers a full day to terminate and test 144 fibers. With MTP connectors, suddenly installers had the ability to rapidly connect 8 to 12 fibers at a time with the snap of a tool, or using a preterminated plug-and-play cable, trimming a daylong job to just a few hours. To ensure seamless connections, the MTP connector was the first MPO connector to be factory-verified and pre-engineered to proper lengths for the cable plant. This meant that less skill was required for installation, while future updates, additions, and changes to the structured cabling were dramatically simplified. Revolutionary at the time, these advancements introduced by the MTP connector eventually became the industry standard.

Faster deployment was one thing. But installers also needed a way to fit more fibers into smaller spaces. MTP connectors addressed this challenge as well. Even before parallel optics gained popularity, installers were struggling to provision high-density applications. MTP connectors made it easier to do exactly that. In place of a 1U housing with duplex connections holding 144 fibers, the MTP housing was capable of holding 864 fibers — six times the capacity. This fiber density made MTP connectors especially well-suited for data centers with serious space constraints and/or massive amounts of cables.

Advancements in the MTP Fiber Connector

With the increasing prevalence of plug-and-play solutions, MTP connectors quickly became the format of choice for data centers, offering an alternative to LC and SC connectors. But the MTP format is more than a niche connector, with advantages that translate across a wide range of technologies beyond parallel optics. Since their launch, MTP connectors have undergone continual improvements that make them the ideal multifiber connector choice for any data center, of any size.

Highly adaptable and flexible, MTP connectors have continued to evolve to meet the emerging needs of installers, data centers, and the organizations that rely on them. Let’s take a brief tour of the key advancements we’ve seen in the MTP format over the past 20 years.

SM MTP Elite Random intermate: MTP insertion loss rate improvement

Lower Insertion Loss

In 1999, US Conec introduced low-insertion-loss MTP Elite connector components. Corning was then able to build on this technology to introduce industry-leading, low-loss, high-density cabling solutions that delivered premier optical performance and reliable signal power. Since then, MTP insertion loss rates have continued to improve, now rivaling loss rates that single-fiber connectors saw just a few years ago.

Superior Stability in Today's MTP MPO Connectors

Simply put, installers need their connectors to work. The earliest versions of the MPO connector format could plug in without problem, but accidental bumps to the cable could result in signal instability. Installers welcomed the introduction of the floating ferrule in the MTP connector. The innovative design allowed the ferrules to stay in contact while the connector housings rotated relative to each other. This major step in the MTP connector’s evolution life allowed multi-fiber connectors to provide even more consistent, reliable performance. The floating ferrule feature was particularly important for applications where the cable plugs directly into an active Tx/Rx device, and was a primary reason the MTP became the connector of choice for emerging parallel optics Tx/Rx applications.

Between 2000 and 2002, additional improvements to the precision of MTP connector components resulted in increased stability and boosted durability performance while continuing to enhance the connectors’ overall reliability. Through countless empirical studies, engineers optimized the lead-in on the precision alignment guide pins to an elliptical shape. This significantly reduced the wear and tear and debris generation from plugging and re-plugging the connector multiple times. In addition, the internal connector components were redesigned to ensure perfectly centered normal forces between the mating ferrules, ensuring physical contact of all polished fiber tips in the ferrule. Finally, installers had a connection that actually stayed connected.

The MTP reputation for performance continues. Used in a variety of applications, today’s MTP connectors meet stringent Telcordia (formerly Bellcore) standards for carrier-grade demands and decades of use. Millions of MTP connectors installed in the field continue to perform as they did when they were first built in the cable assembly factory.

MTP MPO Connectors are Simpler to Make — and Use

In 2002, US Conec migrated MTP’s original thermosetting ferrule technology to polyphenylene sulfide (PPS) thermoplastic injection molding, which is much less susceptible to moisture absorption — a key culprit in degraded connector performance. The adoption of thermoplastic injection molding also made it possible to quickly scale up production to meet high-volume demand, while also improving control over ferrule end-face geometry during the polishing to improve connector performance.

Design improvements to the MTP Elite housing component also made it easier to install, take out, clean, and return to service. This set the stage for future innovations poised to simplify life for installers even more — but more on that later.

Any Technology. Any Data Center. Any Size.

We’ve come a long way since that initial MT ferrule technology used in Japanese telecom networks. But the MTP format is just getting started. Today, the challenge we face is hyperscale, big data, and cloud data centers: How do we provision, add, and support high-density, bandwidth-greedy applications that require massive space to accommodate a massive number of cables? With its ever-improving insertion loss, fiber density, and ease of installation, and its time-tested stability, the MTP connector is ready to meet those demands.

But it’s important to note that the MTP brand isn’t built just for the mega-cloud, big data, and hyperscale computing. The latest versions of MTP connectors are designed to work not only with true fiber-to-fiber connections, but with a host of other technology and electronics across all vertical industries – financial, medical, educational, co-location, and more.

So whether you’re working with duplex, 8-, or 16-fiber transmissions, the MTP connector scales to whatever technology you’re using – including new parallel applications such as 400 Gb Ethernet capable of running across 32, 16, and 8 fibers. With their robust engineering, MTP connectors also perform in a wide range of operating environments, including those with high humidity, extreme heat and cold, and fluctuating temperatures.

The MTP connector scales with whatever technology you’re using – including emerging parallel optics applications such as 400 Gb Ethernet capable of running across 32, 16, and 8 fibers.

Meet the Next-Generation MTP® Connector

With its usefulness in so many different applications with so many different technologies, the MTP connector offers versatility that is definitely an advantage for installers. But this versatility has also presented some challenges. Installers struggle with not knowing whether they need a male or a female end, or with managing polarity when they’re dealing with thousands of fibers that not only have to transmit but also receive. These issues can delay deployment and rack up hours on the job.

The latest generation of the MTP connector brings novel features and functionality that simplify field configurability. Don’t have the right male or female end on hand? Not a problem. These new MTP connectors make it easy to change gender and polarity in the field, without requiring a specialized skill set or a connector engineer. Along with optimized field configurability, the connectors also feature environmentally friendly performance enhancements that improve the feel of plugging and unplugging.

2022 and Beyond, The Evolution of the MTP Connector

For over 20 years, MTP connectors have been relied on to accelerate data center installations, and the next evolution of this technology is the Fast-Track MTP.  As the demand for density, speed and sustainability increases, Corning continues to innovate solutions that fully integrate with our EDGE™ Platform. Take advantage of the time savings, space efficiencies, and simplicity synonymous with the MTP brand; explore the next-generation Fast-Track MTP connector!

Learn more about the Advantages of the MTP connector by downloading our whitepaper.

Ready for design help?

For prompt assistance, please complete the form below and one of our representatives will contact you. 

Thanks you!

Thank you for contacting us. A Corning representative will be contacting you shortly about your inquiry. Should you need immediate assistance please all our customer service line at +1 800-743-2675.