ISCT 2025

Global Showcase Presentations:

Global Showcase Presentations:

Thursday, May 8 10:15 - 10:45 | Theater B

Effective Manufacturing of Allogeneic Mesenchymal Stem Cells Using a Scalable Closed System Circulation Platform

Presenter: Masashi Yamada, Director, Manufacturing Development Dept., S-Quatre Corporation, Japan

Abstract: S-Quatre is enhancing the scalability of SHED (Stem Cells from Human Exfoliated Deciduous Teeth) manufacturing to meet commercial production targets, requiring the generation of billions to trillions of cells per batch. Traditional stacked vessel technology poses challenges in space and labor efficiency, leading to the exploration of Corning’s circulation-based CellCube system. Our data demonstrated that the CellCube system achieves comparable cell density, population doubling time, and MSC marker expression to legacy Corning CellSTACK vessels while offering high scalability and reducing media consumption. This approach effectively addresses scalability challenges and lowers production costs, paving the way for commercial-scale manufacturing.

Thursday, May 8 1:15 - 1:45 | Theater B

Evaluation of the Corning Ascent Fixed Bed Bioreactor System for The Adherent Expansion of Human Induced Pluripotent Stem Cells

Presenter: Misha A. Teale, Research Associate, Zurich University of Applied Science, Wädenswil, Switzerland

Abstract: Allogeneic cell therapy (AlloCT) has gained remarkable clinical and commercial momentum in recent years, offering patients a more affordable, accessible, and sustainable alternative to existing treatment options. Comprehensively characterized following their derivation from consenting and healthy donors, human induced pluripotent stem cells (hiPSCs) serve as a particularly attractive starting point for AlloCT, given their ability to produce a broad range of therapies from a single cell line. Despite their potential, scaling hiPSC expansion processes to meet clinical demand, especially prior to differentiation, remains challenging, as stirred bioreactors, often deemed the most scalable option, may not be universally suitable depending on the target product.

This presentation therefore highlights the evaluation of Corning’s scalable single-use Ascent Fixed Bed Bioreactor System as an alternative for the adherent expansion of hiPSCs, discussing the particulars of process development and comparing its performance to two other single-use bioreactors of a similar scale. Accordingly, our preliminary findings indicate that the Ascent was able to produce over 4.5 billion high-quality hiPSCs within five days at benchtop scale. Such yields, once differentiated, not only enable multi-patient treatment for a range of diseases, but also lay the foundation for further process development work directed at scalable differentiation and industrial production.

Learn More

Join us for Office Hours at ISCT 2025

Join us for Office Hours at ISCT 2025

Stop by our booth (#912) for office hours with our scientific team. This is a unique opportunity to deep dive into several technical topics and get answers to your most pressing questions.

Topics Covered:

  • Efficient characterization of exosomes with product demos (Wednesday, May 7, 1 – 4 PM)
  • Scaling-up and out with stem cells – MSCs and iPSCs (Wednesday, May 7, 5 – 7 PM)
  • Automation for process characterization with the Corning CellCube and Ascent fixed bed bioreactor systems (Thursday, May 8, 11 AM – 1 PM)
  • 3D cell culture models for more effective drug testing (Thursday, May 8, 3 – 5 PM)
  • Considerations for closed systems (Friday, May 9, 12 – 2 PM)

Whether you have specific questions or are just curious to learn more, this is a great chance to get insights straight from the experts. If you can’t make a specific time, please feel free to come by anytime during the show.