How Corning’s Fiber-to-the-Chip Connectivity Solution Will Reduce Data Center Power Consumption While Expanding Bandwidth and Fiber Density
By Benoit Fleury
Published: July 1, 2021
The ever-growing hunger for bandwidth in our ever-more connected society means that fiber optic technology must constantly innovate to ensure that connected enterprises – which increasingly means all enterprises – can continue to meet demand for digital services.
And with high-performance computing and 5G being deployed on a wide scale, data centers must grow their networking speed and capacity even faster.
But with growth comes challenges, and as their capacity increases, data centers are running into a major problem: keeping energy costs under control.
As both fiber optic speeds and switch capacities increase – which is necessary to meet bandwidth needs – more energy is required to transport the electric signal from the point of fiber termination, where the signal changes from light into electricity, to the chip. Carrying a very high-speed signal over an electrical trace is itself extremely energy intensive. That energy creates heat, and thus additional power is needed to keep the data center cool. Thus, the energy use problem gets compounded as additional switches, with many electrical connections, become denser, increasing energy consumption at an unsustainable rate.