Together, Corning and Instrata are helping to secure the future of infrastructure
By Gayla Arrindell and Thinh Phan
Published: July 16, 2026
In today’s hyper-connected world, security infrastructure is defined by the data that powers it.
A new wave of devices—from cameras that perform real-time analysis to IoT sensors—is ushering in an era of smarter, more responsive environments. But this explosion of data has exposed new vulnerabilities in the networks they run on.
Legacy copper networks simply weren’t built to handle the immense bandwidth and speed required by today’s security demands, creating a bottleneck that can undermine the entire system.
To meet this challenge, organizations need to build security from the ground up, with a reliable foundation. That’s the core mission behind the partnership between Corning and Instrata. By combining Corning’s fiber optic infrastructure and Instrata’s leading security expertise, we’re able to deliver a powerful, end-to-end solution designed to meet the demands of today’s security landscape.
Why the security industry is moving to fiber
Fifteen years ago, security meant a remote monitoring station that would receive an alert so personnel could call the police. But security has shifted from passively recording events to creating proactive, intelligent systems that identify threats in real time.
Modern security-as-a-service (SaaS) approaches use cloud platforms to continuously monitor the performance of the security system itself, analyzing data to detect and prevent incidents before they happen. A SaaS model means enormous amounts of high-resolution video and sensor data are constantly being transferred to the cloud for processing and action.
The ability to react to security threats in milliseconds depends entirely on a network that can send and receive signals without delay. To do this effectively, throughput, latency, and bandwidth are more important than ever—and fiber is key to enabling effective integration of new devices.
The power of smarter security
With a fiber network, organizations can reimagine what a security camera can be and what it can do. Cameras have evolved from passive recorders into active, intelligent devices with powerful processing capabilities. With today’s visual intelligence, the system itself can act, reducing manual decision-making and bringing efficiency and speed to the process.