Hospitality Network Solutions | Fiber to the Room | Corning

Redefining Hotel Connectivity for the Future

Fiber to the Room Hospitality Network Solutions

Fiber to the Room Hospitality Network Solutions

For business and leisure travelers alike, reliable connectivity has become the expectation in our increasingly connected world – and when properties struggle to deliver, guest satisfaction and brand loyalty are negatively impacted.

A fiber to the room solution makes multiple, independent copper-based systems – and their costly, disruptive rip-and-replace cycles – a thing of the past. It gives hospitality properties an environmentally friendly network infrastructure that is ideal to accommodate today’s connected device usage and is easily upgradeable to address tomorrow’s hospitality network demands.

With flexible, space-saving options to fit properties of any size, Corning’s hotel-ready, operator-grade, fiber-based hospitality network solutions provide Ethernet and the capacity to meet guest expectations today and deliver next-gen experiences tomorrow.

American Hotel and Lodging Association
Corning is a proud member of the American Hotel and Lodging Association.

Solution Stories

Featured Case Studies

Featured Case Studies

Wigwam Resort Case Study

The Wigwam Resort is a historic Arizona resort in business since 1929. Whether traveling for business, romance, relaxation, or family fun, Wigwam's 440 acres offer a variety of amenities. Corning partnered with Wigwam to deliver a  fiber to the room solution across the property. By addressing challenges presented by the widespread deployment and historic nature of the resort, the project ensured best-in-class connectivity for the resort and its guests.

Project Overview: Wigwam Resort Case Study >>

Resorts World: Unlocking the Potential of a Connected Experience

Corning, along with KLA Labs, helped Resorts World build the largest hotel property the strip had seen in over a decade. With a focus on guest and employee experience, Corning was able bring a fiber-rich, fully integrated network with 5+ connected devices to each room.

Resorts World: Unlocking the Potential of a Connected Experience >>

From The Signal Blog

From The Signal Blog

Fiber to the Slot Machine: Fiber Backs Vegas’ Newest High-Tech Casino Resort

In a city defined by its eye-popping flair, it takes an especially bold effort to stand out from the pack. Since opening in 2021, Resorts World Las Vegas has done just that: as the first new resort property to join the Las Vegas Strip in over a decade, the facility features an array of groundbreaking technologies that take hospitality, gaming, and entertainment to a whole new level—and it’s all made possible by an extensive fiber optic infrastructure.
 

Read More

Creating the Hotel of the Future

Every hotel guest has certain expectations when they book their stay. They expect top tier customer service, affordable prices and ample amenities – and chief among them is fast, reliable Internet. Guests are more likely to complain about shoddy Wi-Fi than delayed room service or a late check-in. Technology in the hospitality space is rapidly evolving, and hospitality companies need to reimagine what the hotel of the future looks like to keep up with visitors' expectations.

Contact Us Today

A member of our team can answer questions about our hospitality portfolio.

Thank you for your submission!

A Corning representative will be contacting you shortly about your inquiry. Should you need immediate assistance please call our customer service line at +49 30 5303 2100.