Pipettes are among the most ubiquitous tools in research labs. The trusty pipette is easy to take for granted, but how you use your pipettes day-to-day and how you maintain them over time can make a big difference on your experiments and your hand and wrist health. Let's take a look at some pipetting best practices with this in mind.
Like other repetitive motions, pipetting can cause occupational injuries. Research has shown that performing more than 300 hours of pipetting per year can increase the risk of hand and shoulder injury. Many laboratory workers spend more than 500 hours a year (about 2 hours each work day) pipetting. That makes it critical to adopt ergonomic practices.
Using poor pipetting techniques can also wreak havoc on experiments. Many of the technique problems that can increase strain on the user's hands and arms can also reduce accuracy and reliability. For example, if you press too hard when applying tips, the tips may be slightly crushed, which can cause accuracy issues, and you'll likely need to use more force to eject the tips after use, which can increase hand strain. Or, if you pipette at an awkward angle, you may draw an incorrect volume of liquid and potentially increase your risk for injuries over time.
Understanding pipetting best practices will set you up for success.