AF: When expanding iPSCs and generating a future master cell bank, you must confirm that the product is robust from vial to vial or clone to clone. The goal is to maintain high yields and continue to meet your chosen quality metrics, whether at small or large scale. Additionally, safety must be ensured.
One of the platforms that can provide this increased robustness is stacked vessels, and at Corning, there are several solutions for this: for example, the CellSTACK®, and HYPERStack®. Here, we increased the surface area to boost the yield from one product and one vessel, which can then be scaled out. This allows you to maintain consistency in your production.
When considering higher yields, we have a new platform, Ascent®, a fixed bed reactor that increases the surface area yet further and allows more consistent production of your iPSC culture.
JW: We have previously tried the CellSTACK, we are currently trying the HYPERStack, and we are considering trying CellCube® with different cells produced in our GMP operation. However, we haven’t yet found a single platform that will suit all of them. As a developer, you have to do your research to see which platform works the best. So far, I have to say the Corning support has been excellent.
AM: As stated, there is variability in the clones and lines of the iPSCs, but there is also variability in the cells that they further differentiate into. Having the flexibility of different platforms can be helpful, particularly for this application. We have been discussing adherent platforms where the cells adhere to the surface and, generally, that surface is coded for iPSCs.
There have been some transitions to aggregate suspension culture; however, a majority of the literature has been published in 2D platforms. There is a much larger base of data and protocols to pull from utilizing those 2D platforms. There may be some application areas and cell types that the iPSCs would differentiate into that may not be supported in a suspension platform. Again, there is value in having different platforms depending on the end goal of the cell therapy process.