In a busy lab, where there's always a lot on your to-do list, thinking through lab waste disposal practices may not seem like a high priority. However, improving your lab waste disposal can be a big opportunity to reduce environmental impact. In addition, a well-designed waste disposal system is a key component of laboratory safety and compliance and could provide other benefits, like cost savings and better organization in the lab.
Let's look at some ways labs can target sustainability through better lab waste disposal practices.
Reduce the Environmental Impact of Lab Waste Disposal with Vendor Recycling Programs
Research labs generate a significant amount of laboratory waste, including the paper and plastic packaging that keeps items sterile until they're used, but it can be surprisingly straightforward to implement recycling and other sustainable practices, even in a lab that generates hazardous waste. For example, some life science suppliers offer recycling programs, which enable labs to return certain items to the manufacturer for recycling.
A number of labs adopting sustainable practices participate in Corning's recycling program, which involves returning tip boxes, sterile wrappers, and other packaging items to Corning for recycling.
Allyson Clappin, the Greater Boston account manager for Corning, explained how the Corning recycling program fits into a lab's workflow. "Labs will typically have one or two large cardboard boxes underneath the culture hoods. While researchers are doing experiments, as they unwrap items individually, they put the wrappers off to one side. When they're all done in the hood, we put them into the boxes underneath."
Serological pipet wrappers, empty tip boxes, and wrappers and Styrofoam packaging for Falcon® tubes are also collected for return to Corning.
Clappin explained how Corning's lab waste disposal program offers flexibility in terms of how and when the boxes are returned, which can change depending on how much recyclable material the lab produces. "The joint box is picked up periodically by Corning. [For the boxes under the hood], labs will just use any cardboard box, print out a shipping label from the website, and send it off."