The process of getting up and running with Elplasia 12K flasks and optimizing the protocol was "smooth and very timely," Dr. Khoja said. "And of course, that was with the help of Corning Applications." The support that Corning Applications scientists provided was "phenomenal" and helped the FibroBiologics team optimize spheroid production in the Elplasia 12K flasks fairly quickly, he said.
As FibroBiologics progressed from early to later preclinical research and began planning for human clinical trials, they required additional spheroids, which exceeded the capacity of the Elplasia 12K flasks.
In pursuit of further scalability, the team at FibroBiologics collaborated with Corning in testing a new product, the Corning Elplasia 48K vessel. This product utilizes the same ULA surface and rounded microcavity geometry at a larger scale to generate approximately 48,000 spheroids per vessel.
"We worked very closely, and they were extremely helpful in helping us optimize and develop a really nice workflow for utilizing the 48K Elplasia vessel," Dr. Khoja said.
As one of the initial testers of the product, FibroBiologics was able to offer feedback to Corning to optimize features and performance characteristics based on their workflow. "Of course, when you're developing a product, a new product, there's always going to be some challenges, and we expected that, and I think Corning expects that as well. And I think, to be honest with you, the process was fairly smooth from iteration to iteration. Corning was very quick at turning around suggested changes based on what we've seen and sending us another iteration to test."
For Dr. Khoja, the Elplasia 48K vessel is essential for FibroBiologics' work. "It's the scalability. For example, we have a 120-patient clinical trial coming up in Australia in early 2026, for which we have to make four and a half million spheroids. There's no other way we could have made those without the availability of the 48K vessel. Yes, we could have used the 12K vessel, which is available, but again, we would have had to use four times as much."