Multiple System Operators (MSOs) networks are evolving, with fiber driving deeper into the network as operators move to a passive HFC network and utilize full fiber to the home deployment in greenfield builds. Corning is ready to help you seize the opportunity in the next evolution of your network, wherever you are on the road to 10G.
Our deep understanding of fiber and HFC networks, and the steps necessary to evolve HFC or transition to full FTTH, enables our customers to best plan the future migration of their network. Our understanding of the path to 10G is based on our years of experience helping MSOs evolve their networks. Whether you want to drive fiber towards a Node+0 or flip a switch on fiber to the home, Corning can deliver.
We’re constantly working to help MSOs increase the velocity and speed of deployments, as well as enable the full capabilities of their networks, while also reducing the total cost of ownership for our customers. This in turn increases MSOs ability to monetize their network across all platforms, including RF Broadband, Inside Plant (ISP) and the coming wave of 5G and 10G. MSOs are faced with tough challenges on how to evolve their networks, and together we create solutions that help MSOs become ready for the demand of today while building for the future of tomorrow.