蜂窝网络解决方案 | 光通信 | 康宁

Corning Announces Sale of Wireless Business to Airspan Technologies

Latest News: IBN Cellular Products

Airspan Networks Holdings LLC (“Airspan”), a leading global provider of wireless network solutions, has acquired the wireless business of Corning Incorporated.  ​

Airspan Announces Agreement To Acquire Corning’s Wireless Business – Airspan​

The following products were acquired by Airspan in this transaction:​

  • Distributed Antenna System​: 6000​ and 6200​
  • Spidercloud 4G and 5G Small Cell Radio Access Network products​

实用物联网

实用物联网:为物联网的到来而规划和设计

在过去几年中,关于物联网 (IoT) 的文章很多,讨论了附加设备数量的爆炸性增长预测及其将给全球业务带来的预期价值。单单增长预测就令人震惊。从本文的图表中可以看出,从 2018 到 2019 年,全球的物联网设备数量增长为 35.2 亿台。

到 2020 年,物联网将包含超过 300 亿台连接设备。了解这些变化将如何影响您的网络。

了解更多

商业地产需要一个主干

商业地产需要一个主干

在智能建筑的讨论中,部署网络基础设施以提高智能设备对建筑物的智能以及提供持久的有线/无线网络的好处得到了很好的解释。然而,对于任何没有实际租赁或经营商业地产 (CRE) 的人来说,有一个维度是一个盲点。此维度需要独立于租户为自己的业务运营构建的任何内容的主干和通信基础架构。此讨论也适用于企业拥有的架构,而不仅仅是商业地产。

了解更多

不要等待 5G

不要等待 5G

在"4G/5G 时代"中,许多企业可能适合长期使用 LTE,不需要额外的 5G 功能。这并不意味着 LTE 最终不会被 5G 取代,它的意思是,对单个网络的融合将发生得更慢,因为 LTE 不会像智能手机出现时的 3G 那样在负载下崩溃。LTE 将与 5G 一起悄然共存,并在未来一段时间内支持我们的需求。

了解更多

Enable outstanding wireless performance with a fiber network

Enable outstanding wireless performance with a fiber network

Did you know that 80% of cellular usage happens indoors? But today’s higher-frequency signals, particularly for 5G, simply won’t penetrate most building materials, including windows. Dead zones aren’t just frustrating, they’re a serious operational problem for businesses.  

The need for reliable, in-building cellular coverage has never been greater. So how can you quickly and cost-effectively get the always-there, high-capacity connectivity your teams and tenants demand? Corning offers a wide range of LAN and SD-LAN fiber networks that enable in-building cellular solutions across wireless services and frequency bands.  

Our portfolio accommodates a broad array of design scenarios to support modular LTE, 5G small cells, and 5G distributed antenna systems (DAS). No matter what kind of cellular overlay you choose, our network solutions will help you reduce space requirements and power consumption while allowing you to easily add carriers and bands as your needs change. Whether you’re equipping 10,000 square feet or the largest stadium, if the wireless coverage requirement is a single operator small cell system or a DAS-driven by OEM macro base stations, we can work with you to design and deploy a network ideally suited to your needs. 

欢迎联系我们!

有问题或需要帮助吗?我们的团队随时为您提供支持。无论您需要产品信息、技术支持,还是其他一般咨询,请联系我们,我们会为您对接合适的资源。填写下方表单,我们会尽快回复您。

感谢您!

我们的康宁团队将尽快查看您的咨询,并及时与您联系。