Growing up in Harrodsburg, KY, Tommy could see the Corning Plant his grandfather helped build from his front door. As a kid, he would cross the street to meet his Dad, a Corning employee, and walk him home after work. He remembers taking a tour of the plant as a Boy Scout and competing in (and winning!) a Corning contest held for the community to create a “safety poster.” He recalls being bitter as his Dad made him split the winnings with his brother — the same brother who is now also a Corning employee. After three generations of working at Corning, it’s safe to say that to The Shirleys, Corning is family.
Tommy began his journey with Corning just two weeks after high school. Today, he is the Facilities & Services Manager for the Harrodsburg Corning Plant. This is one of the facilities that helps create glass for mobile consumer electronics, including Corning® Gorilla® Glass. In addition, he’s also on the CURE team and the fire brigade, as well as the CMMS administrator. He recently was recognized as Corning Distinguished Associate; a high honor within Corning.
“It’s amazing to me how much our glass, manufactured from this little town in Kentucky, impacts the world,” said Tommy. The Corning Harrodsburg Plant is continuously awarded as one of the best places to work by The Kentucky Chamber of Commerce. “It’s definitely the best place to work in Kentucky but I often say, it’s the best place to work in the world. Corning has been very good to me and my family.”