What is Corning’s Long-Reach Solution

Long-Reach Solutions and Their Meaning

Long-Reach Solutions and Their Meaning

Long-Reach solutions refer to technologies and strategies designed to extend the reach and capabilities of communication networks, particularly in scenarios where traditional networking methods may not be sufficient. These solutions are aimed at overcoming the limitations of existing infrastructure and enabling reliable, high-speed communication over extended distances.

Long-Reach solutions can be adapted to various industries and applications, including airports, hotels, higher ed, government projects, and more.

Learn More >

Long-Reach solutions can be easier than you think to add to your existing network or to start from the ground up.

Read our frequently asked questions to help understand this solution

  • What are Corning's Long-Reach solutions?

    Corning’s Long-Reach solutions offer power and fiber in hard-to-reach locations and powering remote connected devices like security cameras, motion detection lights, and other devices that need connectivity at the edge of a network.

  • What are the benefits of Long-Reach solutions?
    • Extended reach, higher data capacity, and enhanced performance.
    • These long-distance power and fiber solutions can deliver high-speed data transmission over 2,000 feet, making them suitable for applications in remote or hard-to-reach locations.
  • How does Corning's Long-Reach technology work?

    ActiFi® composite cable combines copper conductors for power and our single mode fiber for data transmission to a Corning Media converter that transmits the power and information from your PoE device. This provides high quality Corning fiber with your security camera or other device without having to get an additional power source.

Download the FAQ Document to learn more about our Long-Reach Solution

Download

Corning’s Portfolio of Long-Reach Solutions

Corning’s Portfolio of Long-Reach Solutions

Corning’s portfolio of long-reach solutions includes the ActiFi® Hybrid Cable, the CIP (Corning Intelligent Power) Solution, and fiber-fed devices such as the 10G HPoE Media Converters or the end-to-end Touchless Networking Solution.

The map below shows your media converter solution supporting your IT and Security needs in a Long-Reach application

Click “Learn More” below the products, to be directed to the product pages to see how these products work together to provide power and fiber to your PoE devices.

Long-Reach Solutions

NCSSM Case Study

The North Carolina School of Science and Math is a publicly funded STEM based high school that models how a statewide approach to collaboration and the use of physical and virtual spaces can create tremendous innovation in public education. The Morganton campus is a mixture of historic and new buildings, including dorms where students live 24/7. Delivering state-of-the-art technologies seamlessly across the campus was key to creating a safe and collaborative environment for students and faculty.

Download case study today >

Additional Resources

Have more questions on Long-Reach Solutions?

Contact me today by filling out the form.

Thank you for your submission!

We will be in contact with you soon.