Engineering world-class exterior glass solutions, distinguished by their durability, flexibility, and consistent optical clarity.
As much as automobiles have evolved over time, you’d be surprised to learn that automotive window glass hasn’t really changed in nearly 100 years. Until now. The tried and true process of placing a thick plastic laminate between two plies of soda-lime glass is being redefined using Corning glass for automotive exteriors.
Corning® Fusion5® Glass expands into Class 8 heavy-duty applications
Corning Fusion5 Glass is now being applied in Class 8 heavy-duty truck windshields, expanding its use into more demanding operating environments. Mack Trucks’ new Mack® ImpactShield™ windshield marks the first use of Fusion5 Glass in this segment. Read the Mack Trucks announcement
Corning’s exterior glass solutions enable optimized glazing designs for windshields, roofs, and sidelites
When Fusion5 and Gorilla Glass are used together or with conventional soda lime glass, they offer the ability to optimize performance for specific applications.
For the Bold & Rugged: The Mopar® Windshield made with Corning® Gorilla Glass
The windshield with Corning® Gorilla® Glass provides a strong defense against chips, cracks and fractures. It is available as a factory-installed option for new Jeep Wranglers and Gladiators, and authentic Mopar glass replacement for 2007-current Jeep Wranglers (JK and JL) and all Jeep Gladiators (JT).
Join us on our journey. The future of driving is clear.
Please note that warranty claims must be directed to a Mopar part supplier or dealership. Corning does NOT handle any warranty claims.
For all Gorilla Glass windshield warranty questions, please refer to the Mopar Warranty site