Pipette Primer: Types of Pipettes and How to Use Them | Corning Life Sciences

Scientific investigations and clinical work frequently require precise measurements. Pipettes offer a convenient way to measure the variety of liquids that can provide valuable — and actionable — results.

Here's what you need to know about the different types of pipettes, plus guidance on ways to use and care for pipettes.

Types of Standard Pipettes

Several types of pipets are available for typical, everyday use. However, these devices do have their differences.

Serological Pipette

Serological pipettes transfers liquids measured in milliliters, are calibrated to the tip of the pipette, and measures liquids for dispersion and aspiration. Serological pipettes such as Corning® Falcon® Individually Wrapped Serological Pipets and Corning Stripette™ Serological Pipets, are useful for routine cell culture and transferring cell colonies post-harvest. They can also mix reagents, cell suspensions, cell culture media or chemical solutions. Clinically, serological pipettes are frequently used for urinalysis, blood banking, immunology, and hematology.

Browse Our Products

Volumetric Pipette

Also called a bulb or belly pipette, a volumetric pipette like the Corning PYREX® Reusable Glass Volumetric Pipet delivers specific amounts of solution via free drainage. These pipettes are routinely used to create serial and stock solutions. They're also used for titrations and volumetric analysis. Volumetric pipettes are often the go-to pipette for working with cell culture media, analytical solutions, solvents, and organic chemicals.

Browse Our Products

Transfer Pipette

Also called Pasteur or teat pipettes, these disposable, plastic devices transfer small amounts of liquid without risk of cross-contamination. Transfer pipettes, such as Corning's Falcon® Transfer Pipets or Gosselin™ Transfer Pipets can have graduated or smooth barrels and are used for rough measurements. Transfer pipettes are often used with urinalysis, hematology, immunology, and blood banking.

Browse Our Products

Advanced Pipettes

In addition to standard types of pipettes, advanced pipettor versions are available. These pipettes are frequently used for more specific tasks.

Air Displacement Pipette

With this pipette, a small cushion of air exists between the pipettor piston and the liquid you're measuring. Calibrating the piston can ensure the most accurate delivery of specific liquid amounts. Consequently, these highly accurate pipettors work well with a range of typical pipette functions.

Generally, air displacement pipettors, like Corning Lambda™ EliteTouch™ pipettors, deliver small doses of aqueous or non-viscous liquids that must be measured with pinpoint accuracy. Be aware that temperature, atmospheric pressure, and liquid viscosity and density can significantly affect this pipette's performance.

Browse Our Products

Pipette Ergonomics

Pipette Ergonomics

Using pipettes every day can lead to discomfort and injury that could impact your workflow if you aren't maintaining the proper form. Pipette ergonomics — from proper posture to well-designed equipment — can help you avoid these problems.

To set yourself up for success, you should consistently practice good posture:

  • Keep your workstation at a comfortable height.
  • Adjust your chair so you can sit comfortably at your workstation.
  • Keep your wrist relaxed when pipetting.
  • Avoid exerting too much force with your thumb or finger when pipetting.

Advanced Pipette Maintenance

Advanced Pipette Maintenance

Advanced pipettes need daily maintenance to safeguard their performance and accuracy. Follow these five steps to ensure pipette longevity and the validity of your work.

  1. Clean pipettes: Any contamination can invalidate your results. Follow the instructions provided by the manufacturer of your pipettes to ensure you're cleaning your equipment correctly and thoroughly. Be aware that the correct cleaning method may depend on how you use the pipette. In general, be careful not to submerge the pipette. And, if they're particularly dirty, use a brush with soft plastic bristles to scrub away any grime.
  2. Perform a visual inspection of pipettes: Regularly examine your pipettes for any visible signs of damage or corrosion that could negatively impact your results. Look closely at all parts of the pipette for any cracks, early signs of corrosion, or other obvious areas of damage. In addition, test each pipette component. Buttons should be straight with no signs of chemical damage or corrosion.
  3. Test functionality of pipettes: Regularly check your pipettes to ensure they're working correctly. Set the pipette to maximum volume and test how well the button, piston, and ejector move. All movements should be smooth — not difficult or jerky.
  4. Conduct preventive maintenance of pipettes: Fixing problems after they occur isn't enough. Make preventive maintenance and calibration part of your routine. Proper preventive maintenance typically includes replacing parts of the pipette that can wear down, such as seals and o-rings, as well as re-greasing mechanical components. For complete instructions on proper maintenance, refer to the manufacturer's guidelines.
  5. Establish a maintenance protocol: To streamline your workflow, create a system and schedule for maintenance. Make sure it includes all components of proper care, including cleaning, inspections, functional tests, maintenance, and calibration.

Choosing the right pipette for your task, maintaining proper ergonomics when using pipettes, and following a consistent maintenance schedule will help you achieve the best possible performance from all pipette varieties.