Liquid handling techniques such as pipetting play a large role in day-to-day operations in many life science laboratories. Automated liquid handling systems help researchers save time and reduce human error, promoting consistency and repeatability of experiments. Unfortunately, both manual and automated liquid handling processes have traditionally generated large amounts of waste—including plastic pipette tips, tip racks, tubes, and reservoirs, in addition to packaging for these items.
However, recent innovations and new products are making it easier to cut down on liquid handling waste. At Corning Life Sciences, sustainability experts are incorporating strategies like material reduction, the use of regrind plastic in manufacturing, and design for recyclability. Let's explore some of these developments.
What Are Regrind Plastics and How Are They Used?
There are many different types of regrind plastics—including pre-consumer, post-consumer, and post-industrial regrind. Many manufacturing lines at Corning Life Sciences are now reducing their environmental impact by using pre-consumer regrind plastic. Zack Heath, Product Line Manager for pipette tips and microcentrifuge tubes at Corning Life Sciences, explained how this works. Scrap plastic generated during manufacturing is ground up, fed back into the manufacturing process, and used to generate a new part.
While some of Corning's lab products, including Corning® Universal Fit pipet tips and Axygen® HybridRack® pipet tips, are validated to use up to 35% regrind, Heath said, the amount of regrind in the final product varies based on how much scrap is available. "We don't currently have a steady supply of regrind plastic, so the percentage of regrind varies from day to day," he said. Manufacturing lines that regrind their scrap reduce their environmental impact because they use less virgin plastic, and plastic scrap isn't sent into a waste stream.
Todd Gilmore, Senior Product Line Manager for automation tips and reservoirs at Corning Life Sciences, explained, "There's also postconsumer regrind plastic. If somebody were to take one of our racks after it's used and grind it up to make a new part, that would be postconsumer regrind."
Corning isn't currently using postconsumer regrind in liquid handling product lines, but sustainability experts at Corning are exploring ways to use it in the future to limit lab waste. This would be an important step toward circularity, a model in which waste is recaptured after use and returned to the system to be made into new products. Corning also partners with other organizations to divert regrind unable to be used internally to other applications.