Corning has created an alternative that will help you with the cleaning in day one, helping to save time in installation and cost in consumables for the first mating connection. In February 2020, Corning introduced its CleanAdvantage technology.
CleanAdvantage technology consists of two parts:
- Corning’s proprietary technology is implemented at the factory and cleans the entire ferrule, making the connector not only compliant with IEC 61300-3-35, but also giving peace of mind to the installer as no scoping or cleaning in the field is needed before the first mating connection.