Corning Announces Corning® Gorilla® Glass DX and Corning® Gorilla® Glass DX+

News Release

News Release

News Release

News Releases
Gorilla Glass
Corning Announces Corning® Gorilla® Glass DX and Corning® Gorilla® Glass DX+
Corning Announces Corning® Gorilla® Glass DX and Corning® Gorilla® Glass DX+
Corning NY | Corning | July 18, 2018

State-of the-art glass composites complement the legendary toughness of Gorilla Glass to deliver superior antireflective optics and scratch resistance

CORNING, N.Y., July 18, 2018  — Corning Incorporated (NYSE:GLW) today announced two additions to its portfolio of cover glass innovations – Corning® Gorilla® Glass DX and Corning® Gorilla® Glass DX+. Both of these new glass composites feature an antireflective property that vastly improves optical clarity and superior scratch resistance scaled to consumer needs, while maintaining the legendary toughness and touch sensitivity of Gorilla Glass.

These revolutionary new cover glass enhancements follow the introduction earlier today of Corning’s most durable cover glass to date, Corning® Gorilla® Glass 6. An extension of Corning® Gorilla® Glass SR+, both Gorilla Glass DX and Gorilla Glass DX+ glass composites can be used in combination with Corning’s Gorilla Glass products to best address mobile device manufacturers’ design priorities. While currently being adopted primarily for wearable mobile devices, developments are underway to adapt these new glass composites to larger form-factor devices.

“We have surveyed more than 85,000 global consumers* over the past seven years, and we discovered that nearly 50 percent cited readability as a highly desired feature in a cover glass,” said Scott Forester, division vice president, Marketing and Innovation Products, Corning Gorilla Glass. “But we also know that consumers don’t want to sacrifice the scratch resistance and durability that they’ve come to expect.  Gorilla Glass DX and Gorilla Glass DX+ address this challenge by delivering outstanding readability combined with best-in-class scratch resistance and the inherent toughness of Gorilla Glass, making them ideal for today’s advanced mobile displays.”


Comparing the two new composites
Both Gorilla Glass DX and Gorilla Glass DX+ enhance display readability by improving the front surface reflection by 75 percent versus standard glass, and increasing the display contrast ratio by 50 percent with the same display brightness level. These improvements in optical clarity can also lengthen battery life.

A point of differentiation between the two solutions is in the levels of scratch resistance. Gorilla Glass DX features enhanced optics with the same excellent scratch resistance of Gorilla Glass while Gorilla Glass DX+ provides enhanced optics with superior scratch resistance approaching that of alternative luxury cover materials.

Corning continues to lead the cover glass industry it created more than 10 years ago. Today, Corning Gorilla Glass has been designed into more than 6 billion devices across 45 major brands.

*Corning survey from multiple resource including Nielsen and Toluna studies

About Corning Gorilla Glass
Corning Gorilla Glass was launched in September 2007, literally creating the cover glass industry it currently leads. Since its inception, Corning Gorilla Glass has become the cover glass of choice for device manufacturers around the globe. The durable cover glass technology has been designed into more than 6 billion consumer electronic devices by more than 45 major OEMs.  Today, it would be difficult to find a premium handheld device, anywhere in the world, without Corning Gorilla Glass. Formed through Corning’s proprietary fusion draw process and strengthened through an ion-exchange process, Corning Gorilla Glass continues to deliver industry-leading performance and durability with a thin, pristine surface that is ideal for the Mobile Consumer Electronics industry, as well as Automotive and Interior Architecture applications.

Caution Concerning Forward-Looking Statements
This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effects of acquisitions, dispositions and other similar transactions by the Company, the effect of global business, financial, economic and political conditions; tariffs and import duties; currency fluctuations between the U.S. dollar and other currencies, primarily the Japanese yen, New Taiwan dollar, euro, Chinese yuan, and South Korean won; product demand and industry capacity; competitive products and pricing; availability and costs of critical components and materials; new product development and commercialization; order activity and demand from major customers; the amount and timing of our cash flows and earnings and other conditions, which may affect our ability to pay our quarterly dividend at the planned level or to repurchase shares at planned levels; possible disruption in commercial activities due to terrorist activity, cyber-attack, armed conflict, political or financial instability, natural disasters, or major health concerns; unanticipated disruption to equipment, facilities, IT systems or operations; effect of regulatory and legal developments; ability to pace capital spending to anticipated levels of customer demand; rate of technology change; ability to enforce patents and protect intellectual property and trade secrets; adverse litigation; product and components performance issues; retention of key personnel; customer ability, most notably in the Display Technologies segment, to maintain profitable operations and obtain financing to fund their ongoing operations and manufacturing expansions and pay their receivables when due; loss of significant customers; changes in tax laws and regulations including the Tax Cuts and Jobs Act of 2017; and the potential impact of legislation, government regulations, and other government action and investigations.

For a complete listing of risks and other factors, please reference the risk factors and forward-looking statements described in our annual reports on Form 10-K and quarterly reports on Form 10-Q. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

Web Disclosure
In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it uses its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors, or supplemental to information contained in this or other press releases. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.

About Corning Incorporated
Corning (www.corning.com) is one of the world's leading innovators in materials science, with a more than 165-year track record of life-changing inventions. Corning applies its unparalleled expertise in glass science, ceramic science, and optical physics along with its deep manufacturing and engineering capabilities to develop category-defining products that transform industries and enhance people's lives. Corning succeeds through sustained investment in RD&E, a unique combination of material and process innovation, and deep, trust-based relationships with customers who are global leaders in their industries.

Corning's capabilities are versatile and synergistic, which allows the company to evolve to meet changing market needs, while also helping our customers capture new opportunities in dynamic industries. Today, Corning's markets include optical communications, mobile consumer electronics, display technology, automotive, and life sciences vessels. Corning's industry-leading products include damage-resistant cover glass for mobile devices; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for state-of-the-art communications networks; trusted products to accelerate drug discovery and delivery; and clean-air technologies for cars and trucks.

Media Relations Contacts:                          
Sarah Pakyala
(607) 974-4902
pakyalaSI@corning.com

Gabrielle Bailey                              
(607) 974-6394                                              
baileygr@corning.com            

Investor Relations Contact:
Ann H.S. Nicholson
(607) 974-6716
nicholsoas@corning.com

Follow CorningRSS Feeds | Facebook | Twitter | YouTube

 

 

 

share