Let’s start with Quantum Dot (QD) displays. There have been many versions of QD displays, and today, we’re supplying glass for emissive QD displays, which are compelling because they produce brighter whites and blacker blacks.
Corning’s glass portfolio is well-suited to supply two pieces of precision display glass for QD OLED displays – one is a TFT backplane and another that functions as a color filter or color convertor. The result is a stunning display technology that delivers the benefits of OLED in thin form factor, deep blacks and wide viewing angle, but also with enhanced color reproducibility and efficiency from quantum dot materials.
While QD technology is expected to remain in the premium niche for now, we’re confident that Corning has the right display glasses for the job.
MicroLED is similar to QD display technology in the sense that it is an emissive technology. Through individual red, green, and blue LEDs, it can enable an expanded color gamut and true-black tones.  One aspect that sets it apart is the ability to form a sort of mosaic, where panels can be connected to create enormous displays.
Now when it comes to these mosaic displays, glass becomes very important because panels need to be connected with nearly imperceptible seams. When pixels must be placed essentially edge to edge, we lose the space around the border to make the circuit connections that drive electricity through the panel. Glass, and unique glass processing, allows these connections to be made by wrapping around the edge of the panel.
In addition, glass can provide benefits of a dimensionally stable and smooth surface on which to reliably transfer these MicroLEDs, improving efficiency in manufacturing.  We are seeing large MicroLED TVs coming to market and, like QD TVs, they’re premium products and likely to remain niche for a while longer. Some other applications we might see would be public information displays or even wearables. We’re interested to see how this market develops, and we’re ready with great glass solutions.