Corning Expands AI Data Center Connectivity Portfolio with PRIZM® TMT Technology

News Releases
Optical Communications
Corning Expands AI Data Center Connectivity Portfolio with PRIZM® TMT Technology
Corning Expands AI Data Center Connectivity Portfolio with PRIZM® TMT Technology
CORNING, N.Y. | Corning Incorporated | March 11, 2026
Lens technology enables denser, faster, and more resilient AI optical networks at scale.

Corning Incorporated (NYSE: GLW) today announced a collaboration with US Conec to become a licensee of PRIZM® TMT optical ferrule technology, a solution that allows for higher fiber counts in tighter spaces inside data centers. The addition of PRIZM® TMT expands Corning’s full spectrum of high‑density optical connectivity solutions for next‑generation AI networks.

“AI infrastructure is pushing optical connectivity into new and more demanding environments,” said Mike O’Day, Senior Vice President and General Manager of Corning Optical Communications. “By licensing PRIZM® TMT, Corning is strengthening its ability to deliver scalable, fiber‑rich solutions that help customers build larger, faster, and more efficient AI clusters, while aligning closely with the broader industry ecosystem.”

As AI infrastructure scales with new generations of AI chips and larger cluster sizes, data center customers need to connect an increasing number of accelerators in the scale-out portion of the network. Moreover, traditional short-reach copper links will increasingly be replaced with optical in the scale-up portions of the network, driving the number of optical connections to increase into the thousands of fibers per server rack and switch rack.

This transition is driving significantly higher fiber density inside server racks, increasing the importance of connector density, performance, and installation speed. The PRIZM® TMT ferrule addresses these challenges through precision‐aligned microlenses rather than direct fiber‑to‑fiber contact. The expanded beam PRIZM® TMT ferrule technology allows for faster and more reliable installation, greater contamination resistance, and reduction in total cost of ownership – all critical advantages in demanding scale-up and scale-out AI data center deployments. 

Corning will highlight PRIZM® TMT technology at the 2026 Optical Fiber Communication Conference and Exhibition (OFC), March 17-19 in Los Angeles, California. Attendees can learn how the technology supports emerging data center connectivity strategies in Corning’s booth (#1739). 

For more information, visit our products page and media resources center. 

MMC and PRIZM are registered trademarks of US Conec Ltd. For more information, visit Corning’s products page.

About Corning Incorporated  
Corning (www.corning.com) is one of the world's leading innovators in materials science, with a 175-year track record of life-changing inventions. Corning applies its unparalleled expertise in glass science, ceramic science, and optical physics along with its deep manufacturing and engineering capabilities to develop category-defining products that transform industries and enhance people's lives. Corning succeeds through sustained investment in RD&E, a unique combination of material and process innovation, and deep, trust-based relationships with customers who are global leaders in their industries. Corning's capabilities are versatile and synergistic, which allows the company to evolve to meet changing market needs, while also helping our customers capture new opportunities in dynamic industries. Today, Corning's markets include optical communications, mobile consumer electronics, display, automotive, solar, semiconductors, and life sciences.