Measuring Sustainability in the Lab: A Lab Manager's Guide to Sustainability Metrics

越来越多的高校和企业开始关注实验室的可持续发展。要想打造更绿色环保的实验室,首先需要了解实验室的现状。可以通过一些指标来评估实验室各流程对可持续发展的影响,并了解实验室采购活动所产生的影响。

对于实验室主管而言,这些指标有利于他们了解哪些行为和改变最具成效,还有助于评估可持续发展战略的实施效果以及确定调整措施。

以下五大指标可以帮助您评估实验室流程及采购活动的可持续性。

五大实验室可持续性指标

1. 能耗

根据美国环境保护署推行的能源之星计划,能源使用强度 (EUI) 是评估实验室建筑的一项重要指标。EUI是指每年每平方英尺建筑面积的能源消耗量,即建筑物全年的能源消耗总量除以建筑物的总面积。可以将这一计算结果与行业 (即研究实验室) 中位数进行比较,也可用于每年持续跟踪同一建筑物的表现,以了解其能效趋势。

建筑设计以及大楼内实验室的能源使用习惯势必会影响EUI。实验室可以更近一步地使用电表或智能计量插座来测量仪器和设备的实际用电量。如果仪器或设备维护不当,能耗可能会超出预期。跟踪每台仪器的用电量有助于实验室主管及时发现问题。

康宁致力于持续提升生产工厂的能效,连续10年 (2014至2024年) 当选能源之星年度合作伙伴。此外,康宁还在2016年至2024年期间连续荣膺能源之星可持续卓越奖。

Energy Use

2. Usage-related Metrics

Another way to keep track of energy usage by equipment is through metrics that score how often or to what extent the equipment is in appropriate use. For example, a fume hood can use as much energy per day as 3.5 households, but energy usage drops when the sash is closed. To understand whether the sash is appropriately being kept shut when not in use, laboratory managers can use a metric called the fume hood airflow management ratio. This is defined as the ratio of the average flow in cubic feet per minute (cfm) to the minimum flow in cfm when the sash is closed. A higher ratio indicates the hood is kept open more of the time, while a hood that's always closed will have a ratio of 1.

Another heavy energy user is the freezer, which can consume as much energy per day as a single-family home. A freezer that's only 60% full or that's mostly used to store outdated samples no one will ever use isn't making the best use of that energy. Keeping and updating an inventory of samples, evaluating how much of a freezer's space is used, and collaborating with other labs in the building can help you evaluate freezer use and determine whether improvement is necessary.

Cell culture incubators, too, are significant energy users. Process intensification products like the Corning® HYPERFlask cell culture vessel allow researchers to culture more cells per square inch of incubator shelf space, helping labs ensure that the energy consumed by each incubator goes a long way.

Airflow Management

2. 能耗相关指标

跟踪设备能耗的另一种方式就是衡量设备使用的频率或程度。例如,通风橱每天的能耗相当于3.5户家庭的能耗,但调节门关闭时,能耗会大幅下降。实验室主管可以利用通风橱气流管理比值这一度量标准来了解调节门在通风橱未使用时是否已正确关闭,即调节门关闭时的平均流量 (立方英尺/分钟;cfm) 与最小流量的比值。这一比值越高,表明通风橱处于打开状态的时间越长,而对于始终关闭的通风橱,该比值为1。

冰箱是实验室中的另一个能耗大户,它每天的能耗相当于一户家庭的能耗。冰箱空间占用率未达60%或者主要用于存放不再需要的过时样品都属于未充分利用能源。记录并更新样品库存、评估冰箱空间占用率、与大楼内的其他实验室合作,这些举措有助于评估冰箱的使用情况并确定是否需要改进。

细胞培养箱同样是耗电王。利用Corning® HYPERFlask超级细胞培养瓶等过程强化产品,研究人员能够在每平方英寸空间内培养更多细胞,有助于确保每台培养箱消耗的能源都能创造出更大产出。

3. 供应商碳足迹

供应商对可持续发展的承诺不尽相同。寻找已采取行动减少碳排放的供应商有助于实验室减少整体碳足迹。

越来越多的企业根据科学碳目标倡议 (SBTi) 制定碳排放目标。SBTi将碳排放源划分为范围1 (自有设施和车辆产生的直接排放)、范围2 (外购能源产生的排放) 和范围3 (企业采购和使用产品相关的间接排放)。寻找积极致力于实现SBTi目标的合作伙伴是提升实验室可持续性的有效方式。

康宁正通过多种举措以及合作伙伴关系,努力实现宏大的可持续发展目标。2023年,康宁的范围1、范围2以及范围3的减排目标已获SBTi认证。

4. 废弃物产生指标

实验室可以开展废弃物审计,以便了解实验室在一周内产生的可回收物、有害废物和无害废物的数量,并发现减少废弃物和改进回收措施的机会。

如果某一产品会产生大量废弃物,也许可以找到一种可重复使用、产生较少废弃物或使用较少包装的替代产品。有些供应商会推出包装材料或某类废弃物的回收计划。向供应商询问其产品是否使用了可回收材料或降低了材料使用量也是一种非常可取的做法。康宁公司位于世界各地的所有生产工厂和实验室均已获得或正在积极申请ISO 14001认证。这项自愿性标准规定了对环境管理体系 (EMS) 的要求。EMS可确保企业符合相关法律要求,同时还能不断提升企业的环境绩效,如提高能源和资源利用率、减少废弃物。

5. 用水量指标

实验室用水和外购产品的生产用水都会影响实验室的可持续发展。可以制作一张用水量平衡表,记录实验室或大楼中的主要用水流程和设备及其预期用水量。将该表与水费账单进行比较,可从中发现是否有漏水或过度用水的情况。

康宁助您一臂之力

与康宁携手合作,可以让您的实验室更具可持续性。Corning EcoChoice™ 产品采用可持续性设计和生产规范以减少对环境的影响。已纳入该计划的部分产品可通过批量采购和过程强化,减少生产环节的浪费。此外,康宁生命科学旗下75%的工厂均获得2024年度可再生能源证书。北美地区的工厂则可通过康宁回收 (Corning Recycles) 计划,为客户提供简便的报废回收机会。

Water Use

 

Corning Can Help

Working with Corning can help your laboratory become more sustainable. Corning EcoChoice™ products make use of sustainable design and manufacturing practices to reduce environmental impact. Select products included in the program can help reduce your production waste through bulk purchases and process intensification. In addition, 75% of Corning Life Science's plants are covered with Renewable Energy Certificates for 2024. Those in North America can participate in Corning Recycles, a program designed to give customers an easy-to-use end-of-life recycling opportunity.