The optimal choice of technology platform for each of the workflow steps depends on the viral vector being produced and the required scale of the bioproduction. One question associated with cell expansion is whether to grow the cells in an adherent or suspension platform. That decision isn't always straightforward.
"There's a big debate in the field right now about which is the best way to produce viral vectors: with adherent cell culture platforms or with suspension platforms," said Austin Mogen, PhD, a field application scientist at Corning Life Sciences. "Adherent platforms have been well-established for many years, but we are seeing increasing popularity in suspension platforms for multiple reasons. Ultimately, the choice will depend on many factors, including time required for process development, scale, cost, and development of new technologies."
Utilizing adherent vessels at large scale can be challenging due to the historic manual nature of processing adherent cell culture. However, they are also considered the more optimized choice for many cell lines utilized in viral vector production, typically producing higher viral titers than suspension platforms. On the other hand, suspension platforms can provide benefits of scalability and process control, such as implementation of a bioreactor.