Corning expands MiniXtend® portfolio to help solve rising demand for unlimited bandwidth

News Releases
Corporate Communications
Corning expands MiniXtend® portfolio to help solve rising demand for unlimited bandwidth
Corning expands MiniXtend® portfolio to help solve rising demand for unlimited bandwidth
Corning, NY | Corning Incorporated | May 11, 2022

The new MiniXtend HD cables and MiniXtend XD cables deliver even greater density, duct space efficiency and reduced carbon footprint

CORNING, N.Y. — Corning Incorporated today announced the expansion of its popular MiniXtend® cable portfolio, with the introduction of MiniXtend HD cables for 12 to 72 fibres enabling use in microducts with 6 mm inner diameter and MiniXtend XD cables for 192 and 288 fibres.

Corning introduced its MiniXtend cable family to help solve rising demand for unlimited bandwidth capacity and address escalating network duct congestion and convergence as fibre is pushed ever deeper into the network. Designed for installation in microduct systems using air-assisted installation methods, MiniXtend micro cables are up to 50% smaller than standard loose tube cables and offer high fibre counts in a small cable diameter footprint.

The introduction of the MiniXtend HD cables for 12 to 72 fibres and MiniXtend XD cables for 192 and 288 fibres represents the next step in Corning’s ongoing mission to provide solutions that are smaller, denser, easier, and faster to use.

The new cables, soon to be showcased at the annual ANGA COM exhibition in Cologne on May 10-12, also reflect Corning’s commitment to deliver innovations that have the power to drive growth and benefit the environment. In 2021, Corning began to use life cycle assessments performed by third parties to provide industry-recognised calculations of embodied carbon. The reduced diameter cables deliver up to a 20% decreased carbon footprint compared with legacy cables.

  • MiniXtend HD cables deliver a 17% reduction in cable outer diameter, increasing fibre density by 44% and enabling up to 72 fibres in a 6mm ID microduct. The carbon footprint of MiniXtend HD cables is up to 20% lower compared to that of standard MiniXtend cables.
  • The MiniXtend XD cables deliver a 15% reduction in cable outer diameter, increasing headroom in 10 and 12mm ID ducts, as well as enabling up to 192 fibres in 8mm ID and 288 fibres in 10mm ID microducts. The carbon footprint of MiniXtend XD cables is up to 12% lower compared to that of MiniXtend HD cables.

Both cables include Corning’s binderless FastAccess™ Technology, providing up to 70% faster end- and mid-span cable access without the need to use a sharp blade. Uniquely, the MiniXtend HD and XD cables use small grooves to indicate the location of the tear feature, supporting densification.

“Global demand for bandwidth is showing no signs of slowing down, and with more fibres being deployed along more pathways, duct space is becoming more and more congested,” said Dr. Merrion Edwards, director, market & technology development, Corning Optical Fibre and Cable. “With high-density cables now an absolute necessity to support convergence and maximise installation efficiency, the new additions to our MiniXtend family will give Corning customers the tools they need for a smaller footprint today and the simplest path to future growth tomorrow.”

Visitors can experience Corning’s products and demos and find out more at Booth E12 – Hall 8 at ANGA COM 2022. Corning will also showcase its products at the Fiber Connect Council MENA in Dubai on May 16-17 and at the FTTH Conference in Vienna on May 23-25.

For more information, please visit: https://www.corning.com/fiber-to-the-premise/emea/en/home/solutions/minixtend.html

 

About Corning Incorporated

Corning (www.corning.com) is one of the world's leading innovators in materials science, with a 170-year track record of life-changing inventions. Corning applies its unparalleled expertise in glass science, ceramic science, and optical physics along with its deep manufacturing and engineering capabilities to develop category-defining products that transform industries and enhance people's lives. Corning succeeds through sustained investment in RD&E, a unique combination of material and process innovation, and deep, trust-based relationships with customers who are global leaders in their industries. Corning's capabilities are versatile and synergistic, which allows the company to evolve to meet changing market needs, while also helping our customers capture new opportunities in dynamic industries. Today, Corning's markets include optical communications, mobile consumer electronics, display, automotive, and life sciences.

Caution Concerning Forward-Looking Statements

The statements contained in this release that are not historical facts or information and contain words such as “will,” “believe,” “anticipate,” “expect,” “intend,” “plan,” “seek,” “see,” “would,” and “target” and similar expressions are forward-looking statements. These forward-looking statements are made pursuant to the safe harbor provisions of the Private Securities Litigation Reform Act of 1995 and include estimates and assumptions related to economic, competitive and legislative developments. Such statements relate to future events that by their nature address matters that are, to different degrees, uncertain. These estimates are subject to change and uncertainty which are, in many instances, beyond our control. There can be no assurance that future developments will be in accordance with management’s expectations. Actual results could differ materially from those expected by us, depending on the outcome of various factors. We do not undertake to update forward-looking statements. 

Some of the risks, uncertainties and other factors that could cause actual results to differ materially from those expressed in or implied by the forward-looking statements include, but are not limited to: the effects of acquisitions, dispositions and other similar transactions, global business, financial, economic and political conditions; tariffs and import duties; currency fluctuations between the U.S. dollar and other currencies, primarily the Japanese yen, euro, Chinese yuan and South Korean won; product demand and industry capacity; competitive products and pricing; availability and costs of critical components and materials; new product development and commercialization; order activity and demand from major customers; the amount and timing of our cash flows and earnings and other conditions, which may affect our ability to pay our quarterly dividend at the planned level or to repurchase shares at planned levels; possible disruption in commercial activities due to terrorist activity, cyber-attack, armed conflict, political or financial instability, natural disasters, or major health concerns; unanticipated disruption to equipment, facilities, IT systems or operations; effect of regulatory and legal developments; ability to pace capital spending to anticipated levels of customer demand; rate of technology change; ability to enforce patents and protect intellectual property and trade secrets; adverse litigation; product and components performance issues; retention of key personnel; customer ability, most notably in the Display Technologies segment, to maintain profitable operations and obtain financing to fund their ongoing operations and manufacturing expansions and pay their receivables when due; loss of significant customers; changes in tax laws and regulations including the Tax Cuts and Jobs Act of 2017; the impacts of audits by taxing authorities; and the potential impact of legislation, government regulations, and other government action and investigations.

For a complete listing of risks and other factors, please reference the risk factors and forward-looking statements described in our annual reports on Form 10-K and quarterly reports on Form 10-Q.

Web Disclosure

In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it uses its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors, or supplemental to information contained in this or other press releases. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.