How Corning innovations have shaped space exploration
To celebrate World Space Week, which takes place every October, Corning is looking back at our long history of enabling space exploration and discovery.
Close to a century ago, more than three decades before humans traveled into space, Corning was already helping people see farther into the universe.
In 1934, Corning cast the massive 200-inch glass mirror that would become the heart of the Hale Telescope, a project so ambitious that it captured public attention across the United States.
The finished telescope went on to expand humanity's understanding of the universe and established Corning as a trusted partner for some of the world's most demanding optical challenges.
As Corning celebrates its 175th anniversary this year, its nearly century-long role in space exploration stands out as one of the many ways the company has helped enable major milestones in science and discovery. From helping scientists see deeper into the universe to supporting human spaceflight and Earth observation, generations of Corning employees have contributed to missions that continue to expand our understanding of space and our place within it.
"The common thread is always Corning," said David Navan, Product Line Manager, Aerospace & Defense (A&D). "Each generation required a different innovation, but the mission has remained the same: helping people see and understand more."
Today, nearly a century after the Hale Telescope project began, Corning technologies continue helping scientists explore deep space, observe Earth, and support some of the world's most ambitious scientific missions.
Building on a foundation
A major chapter in that story began in 1966, when Corning opened its Canton, New York, facility to manufacture mirrors for telescopes and other advanced optical applications. Over the decades, the facility has grown into a world leader in the glass materials that enable space observation, including Corning® HPFS® Glass (High Purity Fused Silica) and Corning® ULE® Glass (Ultra-Low Expansion). The plant has produced materials for projects including the Subaru Telescope, the Gemini telescopes, and the Discovery Channel Telescope. It has also supported numerous human spaceflight and space exploration programs.
For Mary Edwards, Product Engineer and Program Support Manager, A&D, that story is personal.
Edwards began her career in Canton in the early 1980s, working directly with the specialty glass materials that would support both space-based and ground-based programs.
"I worked as an engineer in the forming department where we make the fused silica and ULE glass," Edwards said.
Over the years, she worked in quality assurance supporting spacecraft-window programs before later contributing to telescope and mirror projects.
While the technologies and tools have advanced dramatically during her career, Edwards said the mindset behind the work has remained largely unchanged. Whether it's a spacecraft window or a telescope mirror, the goal is to carefully control every step of the process and deliver a product that performs exactly as intended.
"It's the material," she said. "And making sure that when you start one, you finish it."
Looking outward
As telescopes grew larger and more sophisticated, the materials and technologies behind them evolved as well.
ULE Glass helped enable missions such as NASA’s Hubble and Kepler space telescopes, both of which transformed astronomers' understanding of the universe. Kepler alone helped identify thousands of planets beyond our solar system, opening a new era in the search for potentially habitable worlds.
More recently, optical technologies engineered and manufactured at Corning's Keene, New Hampshire, facility became part of NASA’s James Webb Space Telescope, the largest and most technically-advanced telescope ever built. These systems help point and stabilize the observatory as it captures views of distant galaxies, stars, and exoplanets. By observing infrared light, Webb allows scientists to look deeper into cosmic history and better understand the origins and evolution of the universe.
Corning also contributed an 11-foot-wide secondary mirror made from ULE Glass to the Vera C. Rubin Observatory in Chile. The Rubin Observatory is currently conducting a decade-long survey of the night sky using the largest digital camera ever constructed. Corning also contributed large fused silica glass for the camera, helping create the largest high-performance optical lens in operation. Rather than producing a collection of still images, the observatory effectively creates a movie of the changing sky, helping researchers identify asteroids, observe supernovae, and investigate major questions about dark matter and the evolution of the universe.
Carrying people into space
Corning's contributions to exploration extend beyond telescopes.
Beginning with NASA's Mercury program in the early 1960s, Corning developed spacecraft windows capable of withstanding the extreme conditions of spaceflight, including dramatic temperature swings, radiation exposure, pressure loads, and impacts from tiny particles traveling at high speeds. Corning glass flew aboard Friendship 7 during John Glenn's historic orbital mission and later played a role in Apollo 11, helping astronauts view the lunar surface before humanity's first moon landing.
Over the decades, Corning's spacecraft-window technologies evolved alongside America's space program.
Edwards remembers hearing firsthand from astronauts who visited the Canton facility.
"Every time an astronaut comes to the plant, they talk about how amazing it is to be able to look back on Earth from up there," she said.
That perspective has shaped more than human spaceflight missions. Corning technologies have also helped scientists study Earth itself from orbit.
In the early 2000s, NASA selected Corning to develop a high-performance optical window for the International Space Station. Installed as part of the Window Observational Research Facility, the window gives astronauts and researchers a uniquely clear view of Earth for photography, environmental monitoring, and scientific observation.
Today, advanced optical systems and hyperspectral imaging technologies continue supporting Earth-observation efforts, helping researchers understand natural resources, environmental change, and conditions across the planet.
The next chapter
As World Space Week highlights the achievements that have shaped modern space exploration, Corning's role in that story spans nearly a century. From the Hale Telescope and Apollo 11 to the James Webb Space Telescope and the Rubin Observatory, the technologies have changed dramatically. What has remained constant is the people behind them.
For Navan, that is the real story.
"There are a lot of smart and dedicated folks that developed these innovations," he said. "These innovations change the world. For our industry, they change how we view the universe."
And as future missions take shape, including some designed to search for Earth-like planets beyond our solar system, Corning's long tradition of solving difficult material- and optical-science challenges continues. The next breakthrough may look very different from the ones that came before it, but it will build on the same foundation of innovation, craftsmanship, and curiosity that has connected generations of Corning employees for nearly a century.