Corning Incorporated (NYSE: GLW) today announced a new solution designed to enable the deployment of in-home optical networks in a non-intrusive, aesthetically appealing manner. The solution is featured at the European FTTH Conference, Feb. 16-18, in Luxembourg.
The Corning® ClearCurve® Invisible Drop Cable solution is built on a foundation of Corning ClearCurve ultra bend-insensitive fiber. The in-living unit kit comes complete with almost-invisible clips and adhesives that are ideal for installation in high-end homes and apartments. ClearCurve Invisible Drop Cable can be attached to walls or ceilings and bent around corners or moldings while preserving critical loss budgets.
“By using ClearCurve Invisible Drop, the visual impact of in-house cabling is dramatically reduced,” said Tobias Schubert, marketing manager, Corning Optical Communications. “Homeowners and residents are given the option of enjoying the benefits of an optical network without having to see it.”
ClearCurve Invisible Drop features standard G.657 fiber, which is compatible with industry connectors and CPEs and can be spliced or connectorized like standard drop cable. The solution requires little training to deploy and can be installed by a single technician. Minimal wall preparation is needed, making installation fast and easy. The single kit offering reduces design and procurement complexity.
For additional information about Corning ClearCurve Invisible Drop Cable, please stop by Corning’s booth (#G14) at the European FTTH Conference in the Luxexpo Exhibition and Conference Centre, Luxembourg.
Forward-Looking and Cautionary Statements
This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.
Digital Media Disclosure
In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it intends to use its website (http://www.corning.com/apac/au/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.
About Corning Incorporated
Corning (www.corning.com) is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives. Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges. Corning’s businesses and markets are constantly evolving. Today, Corning’s products enable diverse industries such as consumer electronics, telecommunications, transportation, and life sciences. They include damage-resistant cover glass for smartphones and tablets; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for high-speed communications networks; trusted products that accelerate drug discovery and manufacturing; and emissions-control products for cars, trucks, and off-road vehicles.