Corning® Guardiant® | Antimicrobial Additive for Paint and Surface Coatings | Corning

Antimicrobial Additive: Copper-Powered Peace of Mind

Corning® Guardiant® is a breakthrough antimicrobial powder additive that can be mixed into paints, coatings, and plastics to impart continuous, long-lasting antimicrobial efficacy. Guardiant leverages copper ion technology that enables products registered with the US Environmental Protection Agency (EPA) to provide supplemental residual sanitizing activity to kill 99.9% of bacteria and viruses within two hours of contact on a painted surface.

The Guardiant Advantage

Products with Guardiant provide unparalleled advantages, addressing the challenges of today as well as tomorrow. Products with Guardiant have been shown to:

 

  • kill a broad spectrum of bacteria and viruses, including the virus that causes COVID-19
  • work continuously with high potency to kill >99.9% of bacteria and viruses in two hours or less
  • provide long term antiviral and antibacterial activity
  • maintain high efficacy under international testing standards and newer testing methods to simulate realistic conditions

Where Can I Use Guardiant as an Additive?

Corning works closely with our customers to develop products with Guardiant-powered antiviral (virucidal) and antibacterial capabilities to benefit homes, hospitals, schools, and more.

Applications

PAINT

Paints powered by Corning Guardiant have been proven to kill bacteria and viruses up to 6 years after the initial application of the paint – which is perfect for high traffic sites such as hospitals, classrooms, and offices.

Learn More

COATINGS

High-traffic areas such as locker rooms and public tranportation facilities can benefit from coatings featuring Guardiant. 

PLASTICS

Plastic materials protected with Corning Guaridant can offer enhanced protection for a wide variety of high-touch surfaces including phone cases, health care products, or products for educational settings. 

Consumer Products

FLOORING

Floors in high-traffic areas can benefit from Guardiant’s antimicrobial  technology – offering peace of mind for those entering and exiting a facility.

 

COUNTERTOPS

Guardiant’s continuous germ-killing capabilities are an excellence feature for frequently utilized countertops for residential, industrial, and health care uses.

MOBILE CONSUMER ELECTRONICS

Phone cases designed with Corning Guardiant can offer antimicrobial protection for devices used in our daily lives. 

Why Copper?

페인트 및 표면 코팅용 새로운 항균 첨가제로 보다 안전한 생활 공간을 만듭니다.

현재 글로벌 보건 위기로 인해 우리 주변의 표면에 존재하는 세균과 바이러스에 대해 그 어느 때 보다 경각심이 높은 상황입니다. 우리는 자주 그리고 철저하게 손을 닦고 손에 닿는 모든 표면을 살균합니다. 그래도 여전히 우리 자신과 가족을 세균으로부터 보호 할만큼 충분하다고 느껴지지는 않습니다. 

오염이 반복해서 발생된다면 오염을 제거하는 것 또한 반복할 수 있지 않을까요? 미 환경보호청(EPA)은 최근 살균제 사용을 보완하는 항균 활동이 내재된 표면의 중요성을 인정한 바 있습니다.   

Corning® Guardiant®는 페인트 및 코팅제에 사용할 수 있는 항균 첨가제입니다. Charles Gerba 박사가 이끄는 아리조나 대학 미생물학 실험실에서 실시한 테스트에 따르면 Corning Guardiant를 함유한 코팅제의 경우, 벽면 및 기타 코팅된 표면에서 코로나19를 일으키는 바이러스를 포함한 세균을 99.9% 사멸 시키는 것으로 나타났습니다.   

Guardiant는 구리의 향균 특성을 활용합니다.

코닝 과학자들은 글라스 매트릭스 내부에 구리 이온을 가두어 유해한 세균을 줄일 수 있는 가장 효과적인 구리 형태를 쉽게 유지하는 유리 조성을 개발했습니다. 코닝은 현재 각 정부 및 규제 요건을 만족하는 Corning Guardiant가 함유된 제품을 개발하기 위해 전 세계 유수 페인트 및 코팅 제조사와 협업하고 있습니다. 미국 내에서 유해 세균에 대한 살균력이 있다고 마케팅 하기 위해서는, Corning Guardiant 함유한 완제품이 먼저 미 환경청(EPA) 에 등록되어야 합니다.  

비디오

*아리조나 대학을 포함한 외부 기관에서 시행된 테스트에 따르면, Corning Guardiant 는 Norovirus, Adenovirus 5, Staphylococcus  aureus, Pseudomonas  aeruginosa,  Escherichia  coli O157H:O7, Methicillin-resistant  Staphylococcus  aureus,  Coronavirus 229E, Influenza A subtype H1N1, SARS-CoV-2를 포함한 세균을 99.9% 사멿시키는 것으로 나타났습니다.