Innovation at a large company like Corning cannot come from just one person or one team; it must be ingrained into the company culture and supported at all levels. Corning has been inventing and innovating for 170 years to meet the needs of an ever-changing world, and it's now applying that same spirit to the climate crisis with the aim of expanding corporate sustainability.
Sustainability Innovators Make Positive Impacts
Corning Life Sciences piloted a Design for Sustainability program in 2022. As Michelle Vessels, Senior Product Manager for Corning Life Sciences Advances Surfaces and 3D explains, "Designing for sustainability means looking at our innovations from conception to launch to see how we can decrease waste and energy use."
For example, Corning® Elplasia® Flasks were designed to use less material and a more energy-efficient manufacturing process when compared to standard molding and assembly procedures. Corning U-shaped cell culture flasks were designed with rounded shoulders that improve usability and allow the flasks to be made with about 23 percent less plastic than traditional T-flasks. Less plastic means fewer emissions associated with plastic resin production and end-of-life incineration.
"Our U-flasks were redesigned to make them mechanically stronger, even though they used less plastic," Vessels says. "The project began as a one-off idea and grew to a whole family of flasks that are very successful for our customers and reduce our plastic usage by millions of pounds per year."
Corning EcoChoice™ products
Corning U-shaped flasks are part of the Corning EcoChoice™ program, which launched in September 2023. EcoChoice products are produced, packaged, and/or distributed in an environmentally friendly manner following U.S. FTC Guidelines. This means that all product sustainability statements are specific, evidence-based, and traceable.
"Corning EcoChoice provides customers more transparency on how their purchasing behaviors impact the environment" explains Sarah Dowdall, Director of Strategy and Sustainability lead. By using EcoChoice products, customers "will also accelerate the life sciences industry towards sustainability—whether through innovation, scale up, or other new ideas."
To be included in the EcoChoice program, products must meet at least one of the following criteria: recycled content (pre-consumer or post-consumer), source reduction, environmental attribute certificates (EACs), or intensification. Intensification means that a product is designed to enable greater cell production per volume of plastic waste.
For example, the multiple layers of Corning HYPERFlask® and HYPERStack® vessels allow more cells to be produced per vessel footprint, which reduces the amount of plastic used per unit of output. To intensify production and reduce plastic usage even more, the Corning Ascent® Fixed Bed Reactor (FBR) System provides something close to a 3D growth environment and ideal conditions for cell growth.
Small Steps Can Yield Big Results
Of course, it's not always appropriate to scale up to reduce plastic waste. There are ways to reduce packaging materials or other factors, even for applications that require single-use virgin plastic. Small savings can add up.
For instance, packaging for Axygen® Brand products has recently been redesigned with recycling in mind. The cartons now feature 100 percent recyclable unbleached natural corrugate, a recyclable aqueous coating, and less ink than the previous design (the ink is now plant-based). All upgraded product packaging is planned to transition by the end of 2024. As another example, reloadable pipette tip boxes are now made with 100 percent recycled polypropylene.