Fortunately, there are solutions to help manufacturers overcome some of these challenges. For example, closed systems for cell production help reduce risk in multiple ways. "The very first reason why people choose closed systems is because they can reduce contamination risk," Tsai said. Closed systems help companies fulfill regulatory and Good Manufacturing Practices (GMP) requirements, she explained, because they eliminate the need for manual manipulation with the cells and culture media.
To reduce manual manipulation, some companies use robotic systems to handle cell culture vessels, Tsai said. "But that can be very costly, especially for a smaller company trying to start a new manufacturing process. In that situation, Corning closed systems can provide a relatively economically-friendly approach for those customers." Furthermore, she said, stackable closed vessels, such as Corning CellSTACK® culture chambers, can be manifolded together using connectors or tube welding, and filling/emptying can include automation via pumps. This saves labor and reduces the potential for human error during handling. Corning's closed system vessels have a proven track record of high performance and reproducibility. In addition, Corning provides supply assurance to mitigate supply-related risks.
According to Sharma, another advantage of Corning's closed systems is consistent surface chemistry. "Starting from the various small-scale vessels like T-flasks up to the largest production scale, Corning provides the same type of surface chemistry. So, for example, if they are growing their cells on a CellBIND surface from the beginning, they do not need to do any process development when they move into a scale-up or a scale-out model."
This plug-and-play aspect of Corning's closed system products enables users to easily change out vessels to meet their needs at various points in the development and manufacturing process, while maintaining reproducibility. For example, a company could perform pre-clinical stage cell biology experiments, scale-up for therapeutic product manufacturing, and relocate manufacturing to a new site, all using Corning vessels with the same surface chemistry, thereby minimizing changes to the cell growth environment.