BEIJING, CHINA – Corning’s Dr. Yi Jiang, Innovation Officer, Corning Greater China, and Business Director, Corning Reactor Technologies, was recently recognized as one of the 2017 recipients of the, ‘Influential Leaders of China's Petroleum and Chemical Industry' award from the China Petroleum and Chemical Industrial Federation (CPCIF) and China Chemical Industry News (CCIN) during the groups’ annual award ceremony earlier this week. He was recognized for his leadership in serving the China chemical industry with Corning’s Advanced-Flow™ reactor (AFR) technology for the last seven years.
AFR technology enables the continuous processing of chemicals with a much smaller footprint and a faster reaction rate than conventional batch reactors. They also provide customers with inherently safer, more cost-effective solutions, specialized engineering support, and process expertise.
"This award means a lot to me personally. It is also a reflection of the efforts of our global AFR team who is extremely customer focused and passionate about growing this product line for Corning in China and around the globe." - Yi Jiang
Yi was one of several individuals from other companies and universities within China to be awarded with this recognition. Corning and Yi were recognized at the same event in 2015 with, “The Most Innovative Enterprises” award as well as the, “Top 10 Entrepreneur” recognitions. In 2016, Corning was awarded with, “The Most Socially Responsible Enterprises” award from the same organizations.
“To be recognized at this ceremony with other impactful leaders within China is a great reflection of the hard work the business team has put into this product line over the past decade,” Yi said. “We’re thrilled that our products are making an impact within the pharmaceutical, fine, and specialty chemical industries and that customers and industry partners see the value that an investment in AFR creates for them.”
Learn more about Corning's AFR technology
Advanced-Flow™ Reactor Products
Low-Flow Reactor
Low-Flow Reactor
Our Low-Flow reactor enables continuous chemical processes in a laboratory while using lower quantities of reactants to run tests.
Our Low-Flow reactor enables continuous chemical processes in a laboratory while using lower quantities of reactants to run tests.
Learn MoreG1 Reactor
G1 Reactor
Corning’s G1 reactor is a flexible unit for a lab or pilot environment that can also be used as a small production unit (up to a few tons per year).
Corning’s G1 reactor is a flexible unit for a lab or pilot environment that can also be used as a small production unit (up to a few tons per year).
Learn MoreG3 Reactor
G3 Reactor
Our G3 reactor retains an outstanding mixing and heat exchange performance while also providing a larger internal volume for full-scale production.
Our G3 reactor retains an outstanding mixing and heat exchange performance while also providing a larger internal volume for full-scale production.
Learn MoreG4 Reactor
G4 Reactor
The G4 reactor is built with ceramic fluidic modules and enables very high flow throughput for large-scale production. It can also be integrated into an existing plant as a cost competitive solution.
The G4 reactor is built with ceramic fluidic modules and enables very high flow throughput for large-scale production. It can also be integrated into an existing plant as a cost competitive solution.
Learn MoreG1 Photo Reactor
G1 Photo Reactor
Corning's G1 photo reactor utilizes the technology of the G1 reactor and the added feature of ultraviolet light to enable photoreactions and a consistent distribution of UV light to chemicals.
Corning's G1 photo reactor utilizes the technology of the G1 reactor and the added feature of ultraviolet light to enable photoreactions and a consistent distribution of UV light to chemicals.
Learn MoreG1 SiC Reactor
G1 SiC Reactor
Corning's G1 SiC reactor is compatible with a wide variety of chemicals – including hydrofluoric acids – and high pH at elevated temperatures.
Corning's G1 SiC reactor is compatible with a wide variety of chemicals – including hydrofluoric acids – and high pH at elevated temperatures.
Learn MoreDosing Lines
Dosing Lines
Corning can provide a suitable dosing system including flow control and a safety valve for Low-Flow to G4 reactors.
Corning can provide a suitable dosing system including flow control and a safety valve for Low-Flow to G4 reactors.
Learn MoreLab Reactor System
Lab Reactor System
Our Lab Reactor is a metal-free plug and play open system that can seamlessly scale-up with other AFR products, and has a photo reactor option.
Our Lab Reactor is a metal-free plug and play open system that can seamlessly scale-up with other AFR products, and has a photo reactor option.
Learn More