Preserving cell viability during cold storage requires carefully balancing the complexities of slowing cellular metabolism while preventing damage caused by cold and freezing to optimize cell storage protocols. Cellular survival depends heavily on the cell's inherent properties, such as membrane composition, growth stage, and its preparation, handling, and storage environment. In this article, we take a closer look at cell storage protocols and cryopreservation best practices, reviewing the key biological, procedural, and environmental factors that influence outcomes during short-term hypothermic storage and long-term cryogenic preservation, as well as practical steps to enhance post-thaw recovery.
Short-Term Cell Storage Protocols
For short-term hypothermic storage at approximately 2–8°C, when metabolism slows but continues, there is an increasing risk of adenosine triphosphate (ATP) depletion, oxidative stress, and osmotic or pH drift. Understanding how biological, procedural, and environmental factors affect storage will help labs take the necessary steps to preserve cell viability during brief cold storage.
Biological Factors in Cell Storage
Cold storage is vital for maintaining effective laboratory workflows and success. However, not all cells respond to cold storage in the same way. Sensitive cell types (neurons/immune cells) are particularly vulnerable, while fibroblasts tolerate lower temperatures more effectively. Even under cold conditions, cells remain metabolically active, leading to ATP depletion and the buildup of reactive oxygen species.
Because these stressors threaten cell survival, it is essential to tailor cell storage protocols according to the cell type. Utilize antioxidants to buffer residual metabolism, minimize hold times before freezing, and closely monitor osmolarity to maintain membrane stability, particularly in sensitive cell lines.
Additionally, the timing of harvesting is critical for successful cryopreservation. Cells in their log growth phase handle cold storage better than cells in the stationary phase. Regular cell counting and viability tests help determine the optimal time for cell harvest. Optimizing each step, from media composition to storage timing, can significantly improve post-thaw recovery and experimental outcomes.
The use of Corning® CoolCell® containers during temporary cold storage can help maintain a controlled cooling environment, as well as ensure uniform cooling, eliminating the need for alcohol or external fluids.
Procedural Factors in Cell Storage
Cell harvesting and handling directly determine post-thaw viability. Overexposure to trypsin or ethylenediaminetetraacetic acid (EDTA) can harm cellular membranes, especially in sensitive cell types.
Using the gentlest dissociation method possible will help limit damage to these sensitive cells. Corning cell scrapers and lifters offer a non-enzymatic alternative to minimize damage during cell harvesting. Minimize pipeting, centrifugation, and sudden temperature changes. Always handle cells with consistent, gentle techniques while maintaining a stable temperature during cold storage preparation. Reducing the time between cell harvest and cryopreservation helps lower metabolic stress.
Planning lab workflows ahead of time can also prevent delays. Use screw-cap tubes to improve environmental sealing during storage and decrease the risk of oxidative damage. Prepare media carefully and always use cold, pre-equilibrated, buffered media, monitoring the media for both pH and osmolarity before use to prevent unnecessary cellular stress.
Maintaining precise environmental conditions is essential during short-term cold storage. Even small temperature fluctuations can disrupt cellular balance. It is therefore essential to monitor storage with digital thermometers and data loggers. In open systems, the loss of carbon dioxide can destabilize the pH.
Sealed containers or CO₂-independent buffers can help maintain a proper pH balance. Osmolarity changes, evaporation, and measurement/precision errors in media preparation may alter media solute levels, stressing cells and lowering viability. Products such as Corning serological pipets can help maintain precision in media preparation.
Additionally, protect cells from UV and fluorescent light by using amber or foil-wrapped containers when possible to prevent DNA damage, and always store cells in dark refrigeration units.
Contamination is another significant and preventable risk. Always use sterile laboratory techniques and containers, such as Corning Falcon® tubes, to minimize chemical and physical stress on the cells, as well as to minimize microbial exposure during storage and handling. Common laboratory contaminants, such as bacteria, fungi, yeast, and especially mycoplasma, as well as cross-contaminating cell lines, necessitate routine screening, aseptic techniques, and reagent validation to maintain a high experimental integrity.
Long-Term Cell Storage Protocols and Cryopreservation Best Practices
Cryopreservation Risks
Cryopreservation is crucial for long-term cell storage. However, it poses several risks. These include:
- Intracellular ice formation remains one of the biggest threats to cellular integrity, particularly for large or vacuolated cells. These cells are also more vulnerable to osmotic shifts and freezing-induced stress. To reduce cryoinjury, use and adjust CPA concentrations according to cell type to avoid toxicity.
- The cell membrane's lipid composition is another crucial factor. High levels of cellular cholesterol or saturated fats decrease membrane fluidity, restricting CPA penetration and raising the risk of freeze-related damage. Proper media mixing and pre-cooling increase the effectiveness of CPAs, while membrane-stabilizing supplements help safeguard sensitive cell lines.
- Long-term cold storage can also impact genetic stability. Stem cells and tumor cell lines are particularly susceptible to chromosomal abnormalities and epigenetic drift. Additionally, freezing may damage mitochondria, impairing energy production and triggering apoptosis post-thaw.
Cryopreservation Protocols
Consistency in cell handling is essential for maximizing and optimizing viability during cryopreservation. Use wide-bore pipet tips to reduce shear stress, and target a cell density of 1-10 million cells/mL. Too few cells may cause damage, while too many can increase CPA toxicity. Adjust seeding density based on cell type and experimental goals. For pre-storage collection, centrifuge cells at <300 × g for under 5 minutes. Excessive force can damage fragile cells, especially after thawing.
Before freezing, allow cells to equilibrate in a CPA for 10–15 minutes at 4°C using cryovials certified for ultra-low storage, such as Corning Cryogenic vials. This ensures proper CPA penetration without prolonged exposure, which could cause toxicity. Maintain a controlled cooling rate of approximately 1°C per minute to minimize the risk of intracellular ice formation. Once frozen, immediately transfer samples to a liquid nitrogen tank (−196°C) for long-term preservation.
Thaw quickly by immersing vials in a 37°C water bath, closely monitoring the process to prevent overheating. Then, quickly dilute the CPA in pre-warmed media and gently centrifuge.
The Importance of Temperature Stability
Temperature stability is essential during the cryogenic storage. Even brief warming above −130°C can cause ice recrystallization, resulting in irreversible cell damage. Recommendations for maintaining temperature stability include:
- Check cryovials for microcracks before use and store tubes upright to minimize physical stress, contamination risk, and leakage.
- Maintain a dry, sterile environment during thawing to control humidity and prevent condensation and contamination.
- Environmental cleanliness should always be a priority. Conduct freezing and thawing procedures within a biosafety cabinet using strict aseptic techniques to prevent microbial and cross-contamination.
Learn more about Corning cryogenic storage solutions and the factors that impact survival from Corning's Survival of the Coolest resource.