Cell therapies are complex treatments with sophisticated requirements for biopharmaceutical process development and manufacturing. Accordingly, laboratories working on cell therapies need to weigh the benefits of in-house production against the benefits of working with a contract development and manufacturing organization, or CDMO.
In-House vs. CDMO Cell Therapy Development Considerations
Cell therapy products are often developed by startups or academic labs that have a narrow pipeline consisting of one or a few products. Many gene and cell therapies under development today need to be custom produced using the patient's cells, and some require separate culture systems for producing viral vectors and for modifying patient-derived or allogenic cells. These factors present unique manufacturing challenges.
Labs weighing whether to pursue in-house production or tap a CDMO have a lot to consider. Here's a look at the advantages and disadvantages that in-house production vs. CDMO cell therapy collaborations offer and some of the factors that can move the needle in either direction.
Related Technology
In cell therapies, small changes in the culture system or process steps can have a big impact, potentially altering cell growth or characteristics. Your lab should plan ahead so that going from pilot scale experiments to production scale, or from preclinical to clinical stages, doesn't require disruptive transitions.
CDMOs offer both process development and manufacturing assistance. Working with an experienced CDMO can allow you to benefit from expensive, specialized equipment and clean room space. If an on-site clean room isn't available, open process steps that require clean rooms can tilt the deck toward working with a CDMO. However, closed culturing systems or automated systems that minimize manual steps may simplify the requirements and make in-house development possible.
Starting with a compatible platform can allow for smooth scale-up to happen in-house. For example, modular and flexible technologies now on the market can help you increase production volumes while maintaining stable conditions for cells.