U.S. Department of Defense Approves Corning® Everon Software-Defined Local Area Network Portfolio for Federal Defense Networks

News Releases
Optical Communications
U.S. Department of Defense Approves Corning® Everon Software-Defined Local Area Network Portfolio for Federal Defense Networks
U.S. Department of Defense Approves Corning® Everon Software-Defined Local Area Network Portfolio for Federal Defense Networks
CORNING, N.Y. | Corning Incorporated | 2024年8月23日

Federal agencies can use Corning technology to build a customizable high-bandwidth network to enable artificial intelligence, 5G connectivity, and more

CORNING, N.Y. (NYSE:GLW) – Corning Incorporated announced today the U.S. Department of Defense’s approval and certification of its Corning Everon® Software-Defined Local Area Network portfolio (SD-LAN) as an Assured Services Local Area Network (ASLAN) by the Joint Interoperability Test Command. The portfolio has been added to the Department of Defense’s Information Network (DoDIN) Approved Products List (APL).

Compatible with other DOD systems, this portfolio enables data-dense applications and streamlined installations, with the capability to evolve as network needs grow. Federal agencies can reduce up to 50% in total cost of ownership compared to a copper-based legacy network, all while achieving a secure and scalable network.

“Current legacy copper infrastructure in most federal facilities simply cannot support future data streams at the speed required for mission success. The rapidly evolving digital capabilities in United States military systems and equipment cannot be hindered or restricted by the limitations of supporting infrastructure which could take years to upgrade,” said Robert Basile, Global Market Development Director, Corning Optical Communications. “Corning's DoDIN APL certification reinforces our commitment to providing solutions for the design and engineering of federal facilities and future networks.”

The Corning Everon® SD-LAN portfolio is an especially vital technology given that high-bandwidth applications, including artificial intelligence, machine learning, and 5G connectivity, are now essential to U.S. national security and other federal missions. Increasingly, agencies and facilities demand an agile network that can adapt in real time and support critical emerging technologies.

Further, Corning’s advanced network orchestration provides seamless visibility and “zero trust” consistent verification of   users, devices, and applications, delivering greater efficiency and more secure operations.  A key benefit of Corning's SD-LAN technology is its easy-to-use, template-based policy system, which can accelerate system audits and updates.

For more information visit our website or visit us at the Department of the Air Force Information Technology and Cyberpower Conference (DAFITC) in Montgomery, Alabama, from August 26-28, 2024, in booth #518.

About Corning Incorporated

Corning (www.corning.com) is one of the world's leading innovators in materials science, with a 170-year track record of life-changing inventions. Corning applies its unparalleled expertise in glass science, ceramic science, and optical physics along with its deep manufacturing and engineering capabilities to develop category-defining products that transform industries and enhance people's lives. Corning succeeds through sustained investment in RD&E, a unique combination of material and process innovation, and deep, trust-based relationships with customers who are global leaders in their industries. Corning's capabilities are versatile and synergistic, which allows the company to evolve to meet changing market needs, while also helping our customers capture new opportunities in dynamic industries. Today, Corning's markets include optical communications, mobile consumer electronics, display, automotive, solar, semiconductors, and life sciences.