Next-generation sequencing (NGS), also called massively parallel sequencing, is a technology that rapidly determines the sequences of millions of DNA or RNA fragments simultaneously. Because of its high speed and low cost compared to other methods, NGS is enabling researchers to gain a greater appreciation of human variation and its links to health, disease, and drug responses.
Recent advancements in NGS have opened up many possibilities in drug discovery and personalized medicine. The roles of these new technologies in drug discovery and medicine span from speeding up the identification of new drug targets to potentially helping clinicians choose the best drug for an individual patient.
Next-Generation Sequencing in Drug Discovery
According to Mars (Xuebin) Wang, Applications Manager at Corning, and Rae (Chia-Jui) Tsai, Ph.D., Genomics & Storage Product Line Manager at Corning, the ability to generate vast amounts of sequence data using NGS has revolutionized the process of identifying potential drug targets. By leveraging electronic health records, researchers can look for associations between genetic variants and specific phenotypes of interest within populations. In population-wide studies, NGS can aid in the discovery of mutations that are likely to cause disease.
Another important role is in target validation. Starting with a candidate drug target, scientists can use NGS to look for people with loss-of-function (LoF) mutations in the gene encoding that drug target. Combining phenotype studies with LoF mutation detection can help scientists confirm the relevance of a target and predict the potential effects of inhibiting that target with a drug.
Once a target is validated, NGS can inform drug design by providing insights into genome structure, genetic variations, gene expression profiles, and epigenetic modifications, Wang and Tsai explained. Once a candidate drug is ready for testing in patients, NGS can aid in the selection of patients for clinical trials of targeted therapies and can enable more precise patient stratification based on genetics within clinical trials. This can lead to smaller, more targeted trials with higher success rates.
NGS combined with innovative disease models, like patient-derived organoids, is also useful for drug repurposing and studying rare diseases. NGS allows for the efficient sequencing of DNA or RNA from organoids, providing valuable genetic and molecular information.