Corning Incorporated (NYSE:GLW) announced that its product portfolio provides full compliance to the newly applied Construction Products Regulation (CPR) for telecommunication cables intended for permanent installation inside of buildings and construction works. Corning’s FREEDM™ B2 gel-free cables and enhanced MIC™ tight-buffered indoor cable family have achieved high-performance B2 and C ratings respectively.
Corning has met the European Union defined uniform classification criteria, which certifies the burn/fire performance of cable throughout Europe. Mandatory 1 July, 2017, products complying with the new requirements need to be marked with a CE label that indicates the cable is both rated according to the standard EN13501-6 and conforms to the fire safety characteristics.
Corning’s updated product portfolio includes high-performance B2 and C rated products which meet recommendations for buildings with high fire risks, such as hospitals, schools, hotels, high-rise buildings/multidwelling units, government or public buildings and data centres.
“Corning is a committed member of the Europacable Association and has maintained a long-term investment in the development and testing of products,” said Matthias Nitschke, cable product line manager for Corning, and the company’s signatory of the Europacable Industry Charter. “CPR will help ensure the circulation of high-quality and safe products in the European market, and we are dedicated to supporting our customers and ultimately improving people’s safety.”
“With the introduction of FREEDM B2 cables, we are proud to provide a product range that meets the highest standards for safety.”
Key benefits of the new FREEDM B2 cables and C-rated MIC cable family include:
FREEDM B2 Cables
- Completely gel-free cable construction which supports the burn behavior in the event of fire by creating less hazardous waste and positively influencing the production of smoke and flaming droplets.
- UV and microbe-resistant LSZH cable jacket with B2 performance, which can be installed in ducts or conduits and requires no re-termination at building entry.
- Suitable for splicing or direct termination (using fan-out tubing), allowing easy cable preparation for short installation times and more accurate results.
- Easily identifiable cable printing and CE labelling on the cable jacket to provide full customer transparency in regards to the cable’s CPR-evaluated performance.
MIC® Tight-Buffered Indoor Cables
- Completely gel-free cable construction.
- Indoor flame-retardant LSZH/FRNC jacket with C performance, suitable for applications with medium to high fire risk and deployable as riser cabling in addition to the cabling between floors.
- Tight-buffered 900 µm construction facilitates easy termination for low-fiber-count applications in the local area network and fiber to the office, which eliminates the need for fan-out kits during installation.
- Easily identifiable cable printing and CE labeling on the cable jacket to provide full customer transparency in regards to the cable’s CPR-evaluated performance.
Additional information on the FREEDM™ B2 gel-free indoor/outdoor cable family and MIC cable family and a full list of certificates is available on the Corning website.
Forward-Looking and Cautionary Statements
This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.
Digital Media Disclosure
In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it intends to use its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.
About Corning Incorporated
Corning (www.corning.com) is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives. Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges. Corning’s businesses and markets are constantly evolving. Today, Corning’s products enable diverse industries such as consumer electronics, telecommunications, transportation, and life sciences. They include damage-resistant cover glass for smartphones and tablets; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for high-speed communications networks; trusted products that accelerate drug discovery and manufacturing; and emissions-control products for cars, trucks, and off-road vehicles.