FAQ 구성 상세 정보
Will there still be repair support for my existing UniCam™ toolkits?
Yes, there will still be repair support for existing UniCam™ toolkits. There are no plans to stop repair support for any UniCam™ toolkits.
FAQ 구성 상세 정보
Why are we making the change?
VoC highlighted improvements that customers wanted within the fiber termination process. Therefore we have enhanced the customer experience and reduced the amount of time to terminate a UniCam® connector by 25 percent. The new tool also provides operational feedback and guidance, resulting in lower labor costs, fewer mistakes, increasing customer profits, and time to do other jobs.
FAQ 구성 상세 정보
What’s different?

There are 45 percent fewer termination steps, from 18 to10. This reduces the time to terminate a UniCam® connector by 25 percent with the new tool. Integrated intelligence provides step-by-step guidance throughout the termination process, as well as corrective guidance in the event that a process error occurs.


Termination guidance is provided by an integrated LCD panel that features Corning® Gorilla® Glass.


The toolkit also includes a 7-in LCD panel with preloaded, step-by-step videos to guide the user through the fiber preparation and termination process.

FAQ 구성 상세 정보
What are the part numbers for the new UniCam™ high-performance toolkit 2?

TKT-UNICAM-PFC2 (Kit)


TL-UCP2 (Installation Tool Only)

FAQ 구성 상세 정보
Are we obsoleting the current UniCam™ high-performance toolkit?
Obsolescence of the current tool kit (TKT-UNICAM-PFC) will be considered in 2018. Regardless, all components within the current PFC toolkit will remain available (a la carte) for the foreseeable future.
FAQ 구성 상세 정보
When will the new UniCam™ high-performance toolkit 2 be available?
Kits are available for shipment to customers now.
FAQ 구성 상세 정보
What is the price difference between the UniCam™ high-performance toolkit and the UniCam™ high-performance toolkit 2?
There is approximately a $450 increase for distributors.
FAQ 구성 상세 정보
When will we start shipping?
Available now.
FAQ 구성 상세 정보
What support resources are available?

UniCam Resource Center


Pioneer training support


Technical support line as needed

FAQ 구성 상세 정보
Are there any promotions?
Ask your local Sales Engineer for promotions surrounding this launch.
FAQ 구성 상세 정보
What is the warranty on the new kit?
The warranty on this kit is 15 months from the manufactured date. The manufactured date is located inside the battery compartment.
FAQ 구성 상세 정보
Is there an exchange program available?
No
FAQ 구성 상세 정보
How do you register the new tool kit?
Customers should visit the UniCam® Registration Page to register your Corning toolkit. URL information is also available on registration card in the kit.
FAQ 구성 상세 정보
Will we offer a gift for registering the new UniCam™ high-performance toolkit 2?
Yes, the gift for the new TKT-UNICAM-PFC2 is a rechargeable AA battery pack that lasts twice as long as conventional batteries and ships directly to customers after the tool kit registration process is complete.
FAQ 구성 상세 정보
Will Corning still offer a gift for registering the older style UniCam™ tools and UniCam™ toolkits?
Yes, the current 2.5 mm port cleaner is still available for the TKT-UNICAM-PFC and TKT-UNICAM.
FAQ 구성 상세 정보
When is the commercial launch?
Commercial launch is February 4, 2018. The launch will coincide with BICSI Winter 2018. It will be heavily promoted at BICSI, through Cabling Installation & Maintenance magazine, Corning loyalty programs, and distributor partners.
FAQ 구성 상세 정보
Is there a UniCam™ high-performance toolkit 2 component reorder guide available?
Yes, the reorder guide is available as the last video on the LCD video panel, or it is available as a PDF as LAN-2013-AEN.
FAQ 구성 상세 정보
Has the UniCam® connector changed?
No, there are no changes to the connector. The focus has been on toolkit enhancements.
FAQ 구성 상세 정보
What is the lead time?
Stock is available at distributors.