Network planning and designing for the arrival of the Internet of Things.
by Art King - Corning Inc.
Appearing In Cabling Installation and Maintenance January 2019
by Art King - Corning Inc.
Appearing In Cabling Installation and Maintenance January 2019
Much has been written about the Internet of Things (IoT) over the last few years, discussing both the explosive growth projections in the number of attached devices and the anticipated value to global business that they will bring. The growth projections alone are staggering. From the chart in this article, you can see that the numerical growth from 2018 to 2019 is 3.52 billion IoT devices globally.
This quantifies what will be asked of IT networking and systems integrators to help attach these devices to various networks, their potential impact, and developing planning guidelines. In the balance of this article, we’ll focus on what’s important to networking professionals as our business customers ask us to add IoT devices to the infrastructure landscape.
To begin, let’s define IoT. IoT is not the desktops, laptops, and tablets we use every day. In general, IoT is the collection of networked devices/applications that are not used by humans, also known as machine-to-machine communications or M2M. They can be sensors that send information, controls that can take action, or both. The devices can operate in homes, office buildings, warehouses, or outdoors from city streets to agricultural fields.
Most IoT devices are standalone and are optimized for their intended usage. To attach an IoT identity to a person, because our smartphones are a “digital mirror” of the owner, there are apps that represent us in the digital space and interact with companion IoT infrastructure. For example, a banking app can be detected when a consumer enters the branch, and the experience with the staff is tailored to them. Finally, there are many apps installed in smartphones that are essentially roving sensors collecting data for much larger IoT platforms.In the infrastructure role of most enterprises, IoT projects will eventually be brought to networking teams by the business units interested in adopting them.
For any IoT usage, there are a few common infrastructure questions to consider:
![]() |
||
| This market projection from Statista indicates the staggering expected growth in worldwide connected devices through 20215. From 2018 to 2019 alone, the growth will be 3.52 billion devices. |
There is a significant number of net- work technologies supported by IoT vendors. IoT vendors will offer the best network technology for their systems, ranging from an Ethernet cable down to wireless low-power wide area (LPWA) service. Since IoT devices ultimately connect to an application, the data traffic from the IoT devices will travel over an IP network, either private or the Internet, to servers in the enterprise data center or in a cloud service like Amazon AWS or Microsoft Azure.
For every network type, planning is necessary to understand the IoT connec- tivity needs are fully satisfied.
In planning and budgeting for IoT, the business that is bringing in the service should be budgeting for all expenses necessary to prepare for them. Network assessments of the target networks are used to develop the additional network improvement budget requirements.
Network design considerations:
For many enterprises, there are economic benefits to architectural convergence of many physical networks onto individual logical network slices sharing the same physical network; yet, each network slice is not connected to or aware of other slices. This design trend is driving an enormous amount of fiber-optic cable being pulled farther towards the edge of networks to enable this “fiber-deep” strategy. How and where IoT leverages it can affect the implementation costs. Please note, we used network slices here as it is an emergent term in 5G that describes logical network
TABLE 1. IoT use cases and network types
Application |
Network Type |
Traffic Volume |
Comments |
Vending machine |
WiFi |
Low |
Unmanaged, not important to enterprise |
Security camera |
Ethernet cable |
High |
Managed by security |
SCADA PLC |
Optical Ethernet |
Low |
Managed by enterprise, mission-critical |
Asset tag |
Cellular or WiFi |
Low |
Unmanaged, important when locating asset |
Industrial robot |
Cellular |
Medium |
Managed by enterprise, mission-critical |
Ankle bracelet |
Cellular IoT |
Low |
Unmanaged |
Field rainfall collector |
LPWA |
Low |
Unmanaged |
Industrial IoT applications in manufac- turing and distribution centers are considered mission critical. In both of these application areas, the interest in replacing wired cable to robots, programmable logic controllers (PLCs), and other networked manufacturing equipment with wireless services is very high.
Wireless enables flexible configurations of the distribution center’s internal conveyor belts that have wired control networks today. High-speed inventory switching is very time-sensitive and requires the high level of network guarantees provided by LTE/5G. Cellular pro- vides time-bound responses, fair access, and quality of service controls.
Wireless enables flexible configurations where the manufacturing line can be reconfigured without the need to restructure wired control networks. Industrial robots that are constantly in-motion and wear out control wiring can have reduced downtime by using LTE/5G for robotic command and control.
Because the downtime in these environments is costly, private LTE or 5G is used to replace the cabling. Private LTE/5G networks are designed to be predictable and don’t use public cellularbecause of the enterprise need for total end-to-end management. When designing IoT networks for these applications, the private LTE/5G network features redundancy in key areas, well-engi- neered coverage throughout the facility, and the necessary capacity to support the demands.
In the industrial cases just mentioned, IoT is managed by the enterprise. In other applications, the enterprise has IoT devices distributed across the enterprise that connect to a cloud service that the enterprise can log into. In these cases, there is no management responsibility for the service, but there is a re- quirement to ensure there is adequate network coverage to support IoT devices anywhere they operate in the enterprise.
For example, every clinical device in a hospital or medical campus may have a built-in wireless module for both locating and transmitting patient data. In many cases, WiFi networks can be used to support these needs, but outdoor needs or clinical devices that accompany first responders will support cellular services. In all these cases the IoT will be managed internally to insure patient data-privacy regulations under the Health Insurance Portability and Accountability Act (HIPAA).
Unmanaged IoT can pose a threat to enterprises where they use the enterprise network to connect to their supporting cloud service.
Examples for your consideration:
All these devices were behind DSL modems, but they were still hacked. Imagine that they were installed on the enterprise network and were connected to the bot army command/control server. What could happen to the inside of the enterprise network in these cases?
Best practices for any devices that are not actively managed by enterprise IT is to never allow them on the enter- prise network. This can be done with Ethernet VLANs and multiple WiFi SSIDs technology to create multiple log- ical network slices sharing the same physical network.
In high-security enterprises, the net- work policy could override creation of a network slice for IoT and require the creation of a parallel physical network to ensure total segregation.
In the U.S., the FCC has developed a revolutionary method for enterprises to ac- cess cellular spectrum that is called Citizens Broadband Radio Service (CBRS). CBRS sets aside 150 MHz of radio spec- trum for use by anyone. CBRS-capable infrastructure requests radio spectrum from a cloud service for use by the enterprise. This access method enables enterprises to build their own private LTE in a building or geographic area without negotiating leased access to radio spectrum from a service provider. Private LTE and, eventually, private 5G offer all the benefits of secure and mission-critical communications while allowing the enterprise the total control required in industrial IoT use cases.
CBRS is close to launching in the U.S., and over the next few years most smartphones and IoT devices are expected to feature CBRS-capable radios. Many enterprises are planning today for CBRS. Information about CBRS can be found at cbrsalliance.org.
The wave of IoT devices and services will drive incremental expansion and capacity increases to existing networks and, in some cases, the creation of segregated IoT overlay networks. Network teams in the enterprise and their systems integrators will be asked to design and plan for the arrival of these IoT devices and networks. A variety of IoT applications may use almost any type of wired and wireless connectivity.
Mission-critical IoT applications will be built and operated by the line of business due to their importance and will open new career opportunities for enterprise IT people. It is a “ground-floor opportunity” to join the transformation.
Want more information?
Learn more: Want more information?We are here to help. Contact us below and we will be in touch.