Corning and University of Liège Announce First Advanced-Flow Reactor Qualified Lab in Europe

Corning and University of Liège Announce First Advanced-Flow Reactor Qualified Lab in Europe

University of Liege Opens Corning AFR Lab

News Releases
企业通信
Corning and University of Liège Announce First Advanced-Flow Reactor Qualified Lab in Europe
Corning and University of Liège Announce First Advanced-Flow Reactor Qualified Lab in Europe
CORNING, N.Y. | Corning Incorporated | 2017年11月3日

The University of Liège in Belgium recently established a Corning Incorporated (NYSE: GLW) Corning® Advanced-Flow™ reactor (AFR) qualified lab at its Center for Integrated Technology and Organic Synthesis (CiTOS). Using AFR technology, the lab provides customers with continuous-flow demonstrations, experimental trials, feasibility testing, and chemical reaction process development.

This is the first qualified lab in Europe to offer AFR testing and process development services. Corning also has AFR-qualified labs in the United States and China. The lab at CiTOS is in close proximity to European customers and enables them to utilize Corning Advanced-Flow reactors.

“This collaboration with CiTOS is great for Corning, as we align with an academic institution that has passion and knowledge around continuous flow processing,” said Alessandra Vizza, regional commercial manager of Corning Reactor Technologies. “They offer expertise for our regional customer base while educating the next generation of chemists and chemical engineers.”

CiTOS specializes in continuous-flow organic chemistry and provides expertise to its customers to perform safe, complex, multi-step sequences; scale up; and fast lab-to-market transitions.

“Becoming the first European Corning Qualified Laboratory is a great honor for us and is the next level for our longstanding collaboration with Corning,” said Jean-Christophe Monbaliu, director of CiTOS. “Having access to Corning’s groundbreaking AFR technologies is definitively a major asset to our laboratory. We are committed to helping customers transition from batch to flow processing and to design scalable, continuous-flow processes as well as promoting flow-chemistry education.”

Corning’s Lab Reactor system, Photo reactor and Low-Flow reactors are available in the CiTOS lab to implement process development and identify appropriate processes that can be easily, safely, and seamlessly transferred to industrial production.

Corning’s AFR technology enables the continuous processing of chemicals with a smaller footprint than conventional batch reactors. They are also specially designed to enable the conversion of batch chemical processes to continuous processes. Corning’s reactors provide customers with cost-effective solutions, specialized engineering support, and process expertise.

Compared with traditional batch reactors, Corning’s reactors can enable at least 100 times enhancement in mixing, 1,000 times improvement in heat transfer performance, and seamless, efficient scale-up from the lab to full-scale production of chemicals for the pharmaceutical, specialty, and fine chemical industries.

Forward-Looking and Cautionary Statements

This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.

Digital Media Disclosure

In accordance with guidance provided by the SEC regarding the use of company websites and social media channels to disclose material information, Corning Incorporated (“Corning”) wishes to notify investors, media, and other interested parties that it intends to use its website (http://www.corning.com/worldwide/en/about-us/news-events.html) to publish important information about the company, including information that may be deemed material to investors. The list of websites and social media channels that the company uses may be updated on Corning’s media and website from time to time. Corning encourages investors, media, and other interested parties to review the information Corning may publish through its website and social media channels as described above, in addition to the company’s SEC filings, press releases, conference calls, and webcasts.

About University of Liège (ULiège), Belgium

Welcoming more than 23,000 students, of whom a quarter are of international origin (134 nationalities), 3,500 teachers and researchers, and offering one of the most diversified educational offers in francophone Belgium (38 bachelor’s degrees, 200 masters degrees, PhDs, numerous in-house training courses), the University of Liège has links with 1,000 institutions world-wide, integrated in vast international academic and scientific networks. ULiège is one of the largest employers in Wallonia (5,000 employees). ULiège also qualifies for European Credit Transfer System (ECTS), DS (Diploma Supplement) and HR Strategy for Researchers (HRS4R) Labels granted by the European Commission, which guarantees the quality of the welcome and follow up support given to exchange students, PhD and Post-doc researchers. Attentive to the needs of society, ULiège plays an important role as a creator of activities with high value added and in providing dynamism to technological centres uniting business companies and public operators (Biotechnologies, Medical Sciences, Space Sciences and Industry, Environment, Agro-Bio Technologies, etc.)

About Corning Incorporated

Corning (www.corning.com) is one of the world's leading innovators in materials science, with a 166-year track record of life-changing inventions. Corning applies its unparalleled expertise in glass science, ceramics science, and optical physics along with its deep manufacturing and engineering capabilities to develop category-defining products that transform industries and enhance people's lives. Corning succeeds through sustained investment in RD&E, a unique combination of material and process innovation, and deep, trust-based relationships with customers who are global leaders in their industries.
Corning's capabilities are versatile and synergistic, which allows the company to evolve to meet changing market needs, while also helping our customers capture new opportunities in dynamic industries. Today, Corning's markets include optical communications, mobile consumer electronics, display technology, automotive, and life sciences vessels. Corning's industry-leading products include damage-resistant cover glass for mobile devices; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for state-of-the-art communications networks; trusted products to accelerate drug discovery and delivery; and clean-air technologies for cars and trucks.